cancel
Showing results for 
Search instead for 
Did you mean: 

Wi-Fi Combo

Anonymous
Not applicable

product that we make is for united state market.

we need under spec.

1. we want to use 1~13 ch.

2. we want to use each mode(b/g/n)

if WICED_COUNTRY_UNITED_STATES is configured then 12, 13 ch can not use

if WICED_COUNTRY_KOREA_REPUBLIC_OF is configured then A connection to a 802.11n-only AP can not be established.

Depending on the country code changes, what is change?

Does anyone have an explanation for the behaviour?

I think that regardless of changing country code, wifi module must establish 802.11n-only ap

I have one more question

    *data = (uint32_t) GMODE_PERFORMANCE;

    retval = wwd_sdpcm_send_ioctl( SDPCM_SET, WLC_SET_GMODE, buffer, 0, WWD_STA_INTERFACE );

after applying upper code, i checked "probe request" packet

but this code dosent apply packet.

and if GMODE_B_DEFERRED, GMODE_ONLY is configured, wifi can not work

thanks

0 Likes
1 Solution
AxLi_1746341
Honored Contributor

FYI,

There is a issue about setting country code to WICED_COUNTRY_KOREA_REPUBLIC_OF

on sdk-3.5.2. (Thought it's reported on a different platform, might be related.)

https://community.broadcom.com/thread/6756

View solution in original post

0 Likes
5 Replies
JoYi_1844281
Contributor II

US not allow WiFi product used Ch 12~14 in 2.4GHz ! it's FCC regulation!

Anonymous
Not applicable

thanks for reply so much

We know fcc regulation that ch 12 ~ 14 is not used

but....

if WICED_COUNTRY_KOREA_REPUBLIC_OF is configured

wifi module can NOT establish ap configured establish 802.11n-only mode

I think that regardless of changing country code, wifi module must establish 802.11n-only mode's ap

Depending on the country code changes, what is changed??

0 Likes
AxLi_1746341
Honored Contributor

coolguy wrote:

but....

if WICED_COUNTRY_KOREA_REPUBLIC_OF is configured

wifi module can NOT establish ap configured establish 802.11n-only mode

Which platform & SDK version are you using?

0 Likes
Anonymous
Not applicable

we use uder info

- wiced version : 3.5.2

- wifi module : BCM43362

- main mcu : stm32f

please answer me my qeustion.

0 Likes
AxLi_1746341
Honored Contributor

FYI,

There is a issue about setting country code to WICED_COUNTRY_KOREA_REPUBLIC_OF

on sdk-3.5.2. (Thought it's reported on a different platform, might be related.)

https://community.broadcom.com/thread/6756

View solution in original post

0 Likes