Dear support,

I have a problem with the debugger not working.

I use an eval board MurataType1LD, It is a combo wifi /ble.

I use WICED studio 4.1 and 43xxx_WiFi SDK.

I use the  the following target : xxx-MurataType1LD-debug download

The download work. After I clicked on the start debug, I go directly to hard fault handler (see in the enclosed file).

Does it do a specific configuration for the debbugger?

Does it do add a specific command in the makefile or in the program?

I configured the debbugger exactly as the documentation(see in enclosed too).

0 Likes
1 Reply
lock attach
Attachments are accessible only for community members.
Anonymous
Not applicable

sorry I forget the enclosed file

0 Likes