Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Wi-Fi Combo Forum Discussions

chch_4469616
Wi-Fi Combo
How do you doI would like to ask if the SDIO of CYW943907AEVAL1F can communicate as a slave device Show More
OlKa_3358896
Wi-Fi Combo
Hi. I working on video streaming based on CYW43907 in Soft AP mode. Unfortunately current WICED release does not support 802.11n in Soft AP mode. So i... Show More
OlKa_3358896
Wi-Fi Combo
Hi. Is it possible start Soft AP on 5GHz Band?I found function wwd_wifi_set_preferred_association_band, but it set band only for Station interface. Show More
OlKa_3358896
Wi-Fi Combo
Hi. I have project with CYW43907 and STM32 for RTSP/RTP video streaming. Video data comes from STM32 by SDIO. Then JPEG frame send to smartphone over ... Show More
MiPa_4537371
Wi-Fi Combo
We are using LBEE5KL1DX Module with external antenna. Due to design and space constraints we are unable to use PCB antenna design used by LBEE5KL1DX M... Show More
agmi_3321141
Wi-Fi Combo
I use scan result to pass to the "wwd_wifi_join_specific" call, but this call fails with reasons like:"1024: Failed to find network","1006: Failed to ... Show More
WaMi_4532936
Wi-Fi Combo
HiWe are looking to update one of our existing products with WiFi & Bluetooth and would prefer an USB interface.Are there any reference designs availa... Show More
CharlesOram
Wi-Fi Combo
Hi,I am using the CYW43012 (or more specifically the Murata Type 1LV module) for a product where the CYW43012 operates as a central and connects to a ... Show More
rimo_4512821
Wi-Fi Combo
I have the STM32MP157C-DK2 eval kit which has a Murara BEE5KL1DX-883 module.  The Murata module incorporates the CYW4343W.  According to Murara the mo... Show More
dera_4529761
Wi-Fi Combo
WiFi chipset Cypress43455 is used with MX8Mmini. This particular chipset supports both AP/ST mode simultaneously.We changed the wpa_supplicant ,hostap... Show More
Forum Information

Wi-Fi Combo

Discussion forum regarding WICED Studio Wi-Fi Combo topics.