Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Wi-Fi Combo Forum Discussions

EyLa_3227556
Wi-Fi Combo
Hello, What  is the correct way to architect dual connectivity scenario (BLE & WiFi) ?I'm using ST32F412+CY4343 combo module and SDK 6.4Can you specif... Show More
MiZh_4707896
Wi-Fi Combo
Hi,The CYW43438 block diagram shows that its Cortex-M3 core has ETM.But I try to read its registers from 0xE0041000, I got all 0xFFFFFFFF.I read it th... Show More
Anonymous
Wi-Fi Combo
Hi,I'm making WWD port to Murata SN8000 with custom board based on STM32F7 (1B SDIO + IRQ).I can succesfully run scan example (FreeRTOS_LwIP_Scan.c), ... Show More
SeFe_4295646
Wi-Fi Combo
This thread was locked a couple weeks ago... Generate an RF test pattern in "production" firmware. but did not end with anything useful for us.However... Show More
KaHi_4747291
Wi-Fi Combo
Hi,I wanted to use some of the peripherals which are under the wiced.platform.MCU.STM32F4xx.peripherals.libraries.src likestm32f4xx_ltdc.cstm32f4xx_i2... Show More
KaHi_4747291
Wi-Fi Combo
Hi,I wanted to use some of the peripherals which are under the wiced.platform.MCU.STM32F4xx.peripherals.libraries.src likestm32f4xx_ltdc.cstm32f4xx_i2... Show More
HaGa_4755126
Wi-Fi Combo
Does murata1LD board support Toshiba 4Gb serial nand flash  with part number TC58CVG2S0HRAIJ?only it can suport nor flash Show More
SrK_4096326
Wi-Fi Combo
Hi,We are working on a project with Murata type1 LD platform(STM32F412RG MCU). On this hardware we wanted to enable one GPIO interrupt which is connec... Show More
NaFi_2915566
Wi-Fi Combo
Is there an API for getting task stats like run time percentage?  The information from tx_thread_info_get() seems to be more related to current status... Show More
EyLa_3227556
Wi-Fi Combo
Hello,There's a bug in aws_mqtt.c (WICED 6.4) when receiving a long messages on a subscribed topic (e.g. AWS CreateKeysAndCertificate provisioning mes... Show More
Forum Information

Wi-Fi Combo

Discussion forum regarding WICED Studio Wi-Fi Combo topics.