Wi-Fi Combo Forum Discussions
Hi. In my project I need to use STM32F427VIT6 with Broadcom wifi radio chip plus external flash to ota upgrade. In Readme.txt I found platform limitation in "Known Limitations & Notes" chapter and there inforamtion that ota upgrade is not possible for STM32F4xx. I invastigated files ".../WICED_SDK/Wiced-SDK-2.3.1/WICED-SDK/Wiced/Platform/common/ARM_Cortex_M4/STM32F4xx/bootloader_ota" and it looks like it should works, so why Readme.txt says that it is impossible? Missing some function for Cortex-M4?
Show Less[WICED_SDK-2.3.1]
Im trying to setup a CA store with wiced_tls_init_root_ca_certificates (taking a valid CA cert from my system), but it fails inside x509parse_crt with error -416.
Unfortunately, there is no source for the SSL library bundled with the SDK (besl?).
Is there an API reference for it somewhere to lookup error codes?
Show Less