Wi-Fi Combo Forum Discussions
Hi.
I am noticing BLE connection problems with the BLE Proximity Reporter application running on ISM43341 hardware with WICED SDK 3.5.1 and LightBlue on iOS 9.2.
Starting WICED v3.5.1
Platform ISM43341_M4G_L44 initialised
Started ThreadX v5.6
Initialising NetX_Duo v5.7_sp2
Creating Packet pools
WWD SDIO interface initialised
WLAN MAC Address : C4:7F:51:80:25:6F
WLAN Firmware : wl0: Oct 13 2014 15:25:13 version 6.10.190.51 (r507746) FWID 01-60cadeb3
00000363 GKI_create_task func=0x8016e29 id=1 name=BTU stack=0x0 stackSize=6144
00000370 GKI_create_task func=0x80182a9 id=0 name=HCISU stack=0x0 stackSize=4096
Unhandled Bluetooth Management Event: 0x15
Bluetooth enabled (success)
Local Bluetooth Address: [43:34:1B:00:1F:AC]
---->>> New ADV state: 3
Waiting for proximity monitor to connect...
GATT connection to [6E:1C:87:98:71:E9] established.
---->>> New ADV state: 0
Local TX power: 4
GATT connection to [6E:1C:87:98:71:E9] released.
---->>> New ADV state: 3
Waiting for proximity monitor to connect...
GATT connection to [6E:1C:87:98:71:E9] established.
---->>> New ADV state: 0
Local TX power: 4
GATT connection to [6E:1C:87:98:71:E9] released.
---->>> New ADV state: 3
Waiting for proximity monitor to connect...
GATT connection to [6E:1C:87:98:71:E9] established.
---->>> New ADV state: 0
Local TX power: 4
GATT connection to [6E:1C:87:98:71:E9] released.
---->>> New ADV state: 3
Waiting for proximity monitor to connect...
GATT connection to [6E:1C:87:98:71:E9] established.
---->>> New ADV state: 0
Local TX power: 4
GATT connection to [6E:1C:87:98:71:E9] released.
---->>> New ADV state: 3
Waiting for proximity monitor to connect...
---->>> New ADV state: 4
---->>> New ADV state: 0
Just wanted to verify if this is a known problem and if there is a workaround.
Show LessThe article described in Creating and/or Editing Debug Configurations shows how to set up the debugger in an earlier version of the WICED IDE. We are using the current version with the 3.4.0 WICED install but are now running under WICED 3.5.0
Version: Luna Service Release 2 (4.4.2)
Build id: 20150219-0600
Can you please provide similar setup instructions to configure the debugger. The settings from the original document have been copied. We are encountering a runtime error when starting gdb complaining about using the --version parameter
Thanks in advance
Show LessThe device not connected over wifi with some access points.
It faild with a dhcp error:
12-29 17:35:44.239 476-1407/system_process E/DhcpStateMachine: DHCP failed on wlan0: Timed out waiting for DHCP to finish
12-29 17:35:44.495 476-545/system_process E/WifiConfigStore: message=DHCP FAILURE
The device connect to some other network correctly.
Not sure it is related but:
The failure access point give ip addresses in the range of 10.0.0.x ...
The success access points give ip address in the range of 196.x... or 172...
Faulier android log while trying to connect to vtech NB403 access point :
01-01 09:12:30.618 475-540/system_process E/WifiConfigStore: saveWifiConfigBSSID Setting BSSID for "sparkup"WPA_PSK to any
01-01 09:12:30.622 475-540/system_process E/WifiStateMachine: Start Disconnecting Watchdog 1
01-01 09:12:30.624 475-540/system_process E/native: do suspend true
01-01 09:12:30.632 174-174/? D/awplayer: <awplayer.cpp:496>: prepareAsync
01-01 09:12:30.632 475-542/system_process D/ConnectivityService: notifyType LOST for NetworkAgentInfo [WIFI () - 100]
01-01 09:12:30.633 475-1304/system_process D/NetworkMonitor/NetworkAgentInfo [WIFI () - 100]: DefaultState{ when=0 what=532487 target=com.android.internal.util.StateMachine$SmHandler }
01-01 09:12:30.633 475-1304/system_process D/NetworkMonitor/NetworkAgentInfo [WIFI () - 100]: Disconnected - quitting
01-01 09:12:30.634 475-475/system_process E/MediaPlayer: Should have subtitle controller already set
01-01 09:12:30.635 475-559/system_process E/MediaPlayer: Should have subtitle controller already set
01-01 09:12:30.635 475-542/system_process E/ConnectivityService: EVENT_NETWORK_INFO_CHANGED from unknown NetworkAgent
01-01 09:12:30.639 174-473/? D/awplayer: <awplayer.cpp:557>: start
01-01 09:12:30.665 174-473/? D/awplayer: <awplayer.cpp:1688>: input invalid args.
01-01 09:12:30.667 170-448/? D/CommandListener: Clearing all IP addresses on wlan0
01-01 09:12:30.674 475-540/system_process E/WifiStateMachine: WifiStateMachine Disconnected CMD_START_SCAN source -2 4, 6 -> obsolete
01-01 09:12:30.676 475-540/system_process D/WifiNetworkAgent: NetworkAgent: NetworkAgent channel lost
01-01 09:12:30.702 174-1332/? W/awplayer: <AudioDec_Decode.c:679>: can't open pFileBs
01-01 09:12:30.707 174-1333/? D/awplayer: <audioRenderComponent.cpp:631>: init sound device.
01-01 09:12:30.707 174-1333/? D/awplayer: <audioRenderComponent.cpp:640>: set sound devide param, sample rate = 48000, channel num = 2.
01-01 09:12:30.710 475-559/system_process D/WindowManager: ******* scanning network ... *******
01-01 09:12:30.712 174-1332/? D/awplayer: <adecoder.c:825>: ==============================pAudioDecoder->pBsInFor->bitrate:2304000
01-01 09:12:30.717 174-1333/? D/awplayer: <awplayer.cpp:3366>: **** audio info, 0, 48000, 2, 2304000
01-01 09:12:30.717 174-1333/? D/awplayer: <player.cpp:2622>: first audio pts = 0
01-01 09:12:30.717 174-1333/? D/awplayer: <audioRenderComponent.cpp:753>: start sound device.
01-01 09:12:30.724 174-1326/? E/awplayer: <CdxWavParser.c:464>: [40;31mCdxStream EOS [0m
01-01 09:12:30.724 174-1326/? W/: <demuxComponent.cpp:2457>: read data from parser return fail.
01-01 09:12:30.724 174-1326/? W/awplayer: <awplayer.cpp:2858>: eos...
01-01 09:12:30.731 174-470/? V/audio_hw_primary: out_set_parameters: routing=2
01-01 09:12:30.731 174-470/? V/audio_hw_primary: adev->out_device is: 2, val is : 2
01-01 09:12:31.100 174-1333/? W/awplayer: <player.cpp:3067>: reset the timer to 0, time difference is -382080
01-01 09:12:31.107 174-470/? V/audio_hw_primary: start_output_stream, line: 739
01-01 09:12:31.107 174-470/? V/codec_audio_pad: headset on is: 0, headphone on is: 0, speaker on is : 2
01-01 09:12:31.107 174-470/? V/codec_audio_pad: in normal mode, headset or speaker on,****LINE:112,FUNC:set_normal_path
01-01 09:12:31.107 174-470/? V/audio_hw_primary: normal mode , speaker,****LINE:664,FUNC:select_output_device
01-01 09:12:31.107 174-470/? V/audio_hw_primary: start_output_stream: card:0, port:0, rate:44100
01-01 09:12:31.108 174-470/? V/audio_hw_primary: do not use out resampler
01-01 09:12:31.251 174-1333/? W/awplayer: <player.cpp:3067>: reset the timer to 46437, time difference is -104861
01-01 09:12:32.529 174-1333/? D/awplayer: <awplayer.cpp:3066>: player notify eos.
01-01 09:12:32.711 475-559/system_process D/WindowManager: ---------------- before start cooee !!! 2s delay ----------------
01-01 09:12:32.711 475-559/system_process D/WindowManager: ---------------- start my_test ----------------
01-01 09:12:32.750 1338-1338/? W/busybox: type=1400 audit(0.0:7): avc: denied { sys_ptrace } for capability=19 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
01-01 09:12:32.770 1338-1338/? W/busybox: type=1400 audit(0.0:8): avc: denied { sys_ptrace } for capability=19 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
01-01 09:12:32.770 1338-1338/? W/busybox: type=1400 audit(0.0:9): avc: denied { sys_ptrace } for capability=19 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
01-01 09:12:32.770 1338-1338/? W/busybox: type=1400 audit(0.0:10): avc: denied { sys_ptrace } for capability=19 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
01-01 09:12:32.770 1338-1338/? W/busybox: type=1400 audit(0.0:11): avc: denied { sys_ptrace } for capability=19 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
01-01 09:12:32.770 1338-1338/? W/busybox: type=1400 audit(0.0:12): avc: denied { sys_ptrace } for capability=19 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
01-01 09:12:32.770 1338-1338/? W/busybox: type=1400 audit(0.0:13): avc: denied { sys_ptrace } for capability=19 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
01-01 09:12:32.770 1338-1338/? W/busybox: type=1400 audit(0.0:14): avc: denied { sys_ptrace } for capability=19 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
01-01 09:12:32.770 1338-1338/? W/busybox: type=1400 audit(0.0:15): avc: denied { sys_ptrace } for capability=19 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
01-01 09:12:32.770 1338-1338/? W/busybox: type=1400 audit(0.0:16): avc: denied { sys_ptrace } for capability=19 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
01-01 09:12:32.770 1338-1338/? W/busybox: type=1400 audit(0.0:17): avc: denied { sys_ptrace } for capability=19 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
01-01 09:12:32.770 1338-1338/? W/busybox: type=1400 audit(0.0:18): avc: denied { sys_ptrace } for capability=19 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
01-01 09:12:32.770 1338-1338/? W/busybox: type=1400 audit(0.0:19): avc: denied { sys_ptrace } for capability=19 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
01-01 09:12:32.770 1338-1338/? W/busybox: type=1400 audit(0.0:20): avc: denied { sys_ptrace } for capability=19 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
01-01 09:12:32.770 1338-1338/? W/busybox: type=1400 audit(0.0:21): avc: denied { sys_ptrace } for capability=19 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
01-01 09:12:32.770 1338-1338/? W/busybox: type=1400 audit(0.0:22): avc: denied { sys_ptrace } for capability=19 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
01-01 09:12:32.770 1338-1338/? W/busybox: type=1400 audit(0.0:23): avc: denied { sys_ptrace } for capability=19 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
01-01 09:12:32.770 1338-1338/? W/busybox: type=1400 audit(0.0:24): avc: denied { sys_ptrace } for capability=19 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
01-01 09:12:32.770 1338-1338/? W/busybox: type=1400 audit(0.0:25): avc: denied { sys_ptrace } for capability=19 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
01-01 09:12:32.770 1338-1338/? W/busybox: type=1400 audit(0.0:26): avc: denied { sys_ptrace } for capability=19 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
01-01 09:12:32.770 1338-1338/? W/busybox: type=1400 audit(0.0:27): avc: denied { sys_ptrace } for capability=19 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
01-01 09:12:32.770 1338-1338/? W/busybox: type=1400 audit(0.0:28): avc: denied { sys_ptrace } for capability=19 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
01-01 09:12:32.770 1338-1338/? W/busybox: type=1400 audit(0.0:29): avc: denied { sys_ptrace } for capability=19 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
01-01 09:12:32.770 1338-1338/? W/busybox: type=1400 audit(0.0:30): avc: denied { sys_ptrace } for capability=19 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
01-01 09:12:32.770 1338-1338/? W/busybox: type=1400 audit(0.0:31): avc: denied { sys_ptrace } for capability=19 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
01-01 09:12:32.770 1338-1338/? W/busybox: type=1400 audit(0.0:32): avc: denied { sys_ptrace } for capability=19 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
01-01 09:12:32.770 1338-1338/? W/busybox: type=1400 audit(0.0:33): avc: denied { sys_ptrace } for capability=19 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
01-01 09:12:32.780 1338-1338/? W/busybox: type=1400 audit(0.0:34): avc: denied { sys_ptrace } for capability=19 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
01-01 09:12:32.780 1338-1338/? W/busybox: type=1400 audit(0.0:35): avc: denied { sys_ptrace } for capability=19 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
01-01 09:12:32.780 1338-1338/? W/busybox: type=1400 audit(0.0:36): avc: denied { sys_ptrace } for capability=19 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
01-01 09:12:32.780 1338-1338/? W/busybox: type=1400 audit(0.0:37): avc: denied { sys_ptrace } for capability=19 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
01-01 09:12:32.780 1338-1338/? W/busybox: type=1400 audit(0.0:38): avc: denied { sys_ptrace } for capability=19 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
01-01 09:12:32.780 1338-1338/? W/busybox: type=1400 audit(0.0:39): avc: denied { sys_ptrace } for capability=19 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
01-01 09:12:32.780 1338-1338/? W/busybox: type=1400 audit(0.0:40): avc: denied { sys_ptrace } for capability=19 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
01-01 09:12:32.780 1338-1338/? W/busybox: type=1400 audit(0.0:41): avc: denied { sys_ptrace } for capability=19 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
01-01 09:12:32.780 1338-1338/? W/busybox: type=1400 audit(0.0:42): avc: denied { sys_ptrace } for capability=19 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
01-01 09:12:32.780 1338-1338/? W/busybox: type=1400 audit(0.0:43): avc: denied { sys_ptrace } for capability=19 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
01-01 09:12:33.416 174-470/? I/AudioFlinger: BUFFER TIMEOUT: remove(4096) from active list on thread 0xb54d8000
01-01 09:12:35.621 174-470/? D/audio_hw_primary: out_standby
01-01 09:12:38.000 1170-1213/com.android.calendar D/InitAlarmsService: Clearing and rescheduling alarms.
01-01 09:12:38.044 475-548/system_process I/ActivityManager: Killing 1152:com.android.settings/1000 (adj 15): empty #7
01-01 09:12:42.727 475-559/system_process D/WindowManager: ---------------- start cooee !!! 10s delay ----------------
01-01 09:12:42.729 475-559/system_process D/lgh: sparkup
01-01 09:12:42.729 475-559/system_process D/lgh: 1234567890
01-01 09:12:42.729 475-559/system_process D/lgh: wpa2
01-01 09:12:42.730 475-559/system_process D/lgh: wifi_security_type = 3
01-01 09:12:42.730 475-559/system_process D/WindowManager: ---------------- go to connect ap !!! ----------------
01-01 09:12:43.730 475-559/system_process D/WindowManager: ---------------- after get wifi.txt 1s delay ----------------
01-01 09:12:43.744 475-540/system_process E/WifiConfigStore: removeNetwork 0 key="sparkup"WPA_PSK config.id=0 crc=2151773480
01-01 09:12:43.759 475-559/system_process E/addOrUpdateNetwork: uid = 1000 SSID "sparkup" nid=-1
01-01 09:12:43.768 475-540/system_process E/WifiConfigStore: key="sparkup"WPA_PSK netId=-1 uid=1000/0
01-01 09:12:43.775 475-540/system_process E/WifiConfigStore: addOrUpdateNetworkNative created netId=0
01-01 09:12:43.850 475-540/system_process E/WifiConfigStore: created new config netId=0 uid=1000
01-01 09:12:43.850 475-540/system_process E/WifiConfigStore: will read network variables netId=0
01-01 09:12:43.858 475-540/system_process E/WifiConfigStore: rewrite network history for "sparkup"WPA_PSK
01-01 09:12:43.866 475-540/system_process E/WifiConfigStore: rewrite network history for "sparkup"WPA_PSK
01-01 09:12:43.867 475-540/system_process E/WifiConfigStore: saveWifiConfigBSSID Setting BSSID for "sparkup"WPA_PSK to any
01-01 09:12:43.959 475-559/system_process I/System.out: a--0
01-01 09:12:43.960 475-559/system_process I/System.out: b--true
01-01 09:12:43.960 475-559/system_process D/WindowManager: ---------------- make wifi coonect only once !!! ----------------
01-01 09:12:43.969 174-547/? E/MediaPlayerFactory: <MediaPlayerFactory.cpp:112>: [40;31mObtain calling process failed [0m
01-01 09:12:43.969 174-547/? D/awplayer: <version.h:26>:
01-01 09:12:43.969 174-547/? D/awplayer: >>>>>>>>>>>>>>>>>>>>>>>>>>>>> CedarX 2.0 <<<<<<<<<<<<<<<<<<<<<<<<<<<<<
01-01 09:12:43.969 174-547/? D/awplayer: version: 2.1.
01-01 09:12:43.969 174-547/? D/awplayer: svn repo:''
01-01 09:12:43.969 174-547/? D/awplayer: last change date:
01-01 09:12:43.969 174-547/? D/awplayer: author: guoshaomin
01-01 09:12:43.969 174-547/? D/awplayer: ----------------------------------------------------------------------
01-01 09:12:44.003 174-547/? D/awplayer: <awplayer.cpp:353>: setDataSource(fd), fd=17
01-01 09:12:44.007 174-547/? D/awplayer: <awplayer.cpp:514>: prepare
01-01 09:12:44.012 174-1349/? D/awplayer: <CdxParser.c:570>: source uri 'fd://19?offset=0&length=330810'
01-01 09:12:44.012 174-1349/? D/awplayer: <CdxFileStream.c:500>: local file 'fd://19?offset=0&length=330810'
01-01 09:12:44.012 174-1349/? D/awplayer: <CdxFileStream.c:427>: (20/0/330810) path:'file:///system/media/wifi_level_good.mp3'
01-01 09:12:43.960 547-547/? W/Binder_2: type=1400 audit(0.0:110): avc: denied { search } for name="475" dev="proc" ino=416 scontext=u:r:mediaserver:s0 tcontext=u:r:system_server:s0 tclass=dir permissive=0
01-01 09:12:43.960 547-547/? W/Binder_2: type=1400 audit(0.0:111): avc: denied { search } for name="475" dev="proc" ino=416 scontext=u:r:mediaserver:s0 tcontext=u:r:system_server:s0 tclass=dir permissive=0
01-01 09:12:44.053 174-1349/? D/awplayer: <CdxFileStream.c:453>: :16:[52 49 46 46 32 0c 05 00 57 41 56 45 66 6d 74 20]
01-01 09:12:44.053 174-1349/? D/awplayer: <CdxFileStream.c:344>: redriect url 'file:///system/media/wifi_level_good.mp3'
01-01 09:12:44.062 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.062 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.062 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.062 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.062 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.062 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.062 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.062 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.062 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.062 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.063 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.063 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.063 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.063 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.063 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.063 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.063 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.063 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.063 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.063 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.063 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.063 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.063 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.063 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.063 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.063 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.063 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.063 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.063 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.063 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.063 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.064 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.064 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.064 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.064 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.064 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.064 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.064 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.064 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.064 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.064 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.064 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.064 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.064 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.064 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.064 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.064 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.064 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.064 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.064 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.064 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.064 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.064 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.065 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.065 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.065 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.065 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.065 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.065 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.065 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.065 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.065 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.065 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.065 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.065 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.065 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.065 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.065 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.065 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.065 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.065 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.065 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.065 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.065 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.065 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.065 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.065 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.065 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.066 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.066 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.066 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.066 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.066 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.066 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.066 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.066 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.067 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.067 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.067 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.067 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.067 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.067 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.067 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.067 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.067 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.067 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.067 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.067 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.067 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.067 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.067 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.067 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.067 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.067 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.067 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.067 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.067 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.067 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.068 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.068 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.068 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.068 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.068 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.068 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.068 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.068 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.068 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.068 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.068 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.068 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.068 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.068 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.068 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.068 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.068 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.068 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.068 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.068 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.068 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.068 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.068 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.068 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.068 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.068 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.069 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.069 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.069 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.069 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.069 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.069 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.069 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.069 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.069 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.069 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.069 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.069 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.069 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.069 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.069 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.069 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.069 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.069 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.069 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.069 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.069 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.069 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.069 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.069 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.069 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.070 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.070 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.070 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.070 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.070 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.070 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.070 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.070 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.070 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.070 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.070 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.070 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.071 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.071 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.071 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.071 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.071 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.071 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.071 174-1349/? W/CdxMp3Parser: <CdxMp3Parser.c:1654>: giving up at offset 65536
01-01 09:12:44.071 174-1349/? W/awplayer: <CdxRemuxParser.c:622>: not privite remux file...
01-01 09:12:44.071 174-1349/? E/CdxFlvParser.c: <CdxFlvParser.c:3848>: [40;31mFlvProbe failed. [0m
01-01 09:12:44.071 174-1349/? E/CdxAviParser: <CdxAviParser.c:1250>: [40;31mAviProbe failed. [0m
01-01 09:12:44.071 174-1349/? D/CdxHlsParser: <CdxHlsParser.c:2204>: HlsParserProbe = 0
01-01 09:12:44.071 174-1349/? D/awplayer: <CdxMkvParser.c:1145>: mkv probe
01-01 09:12:44.071 174-1349/? E/CdxPmpParser: <CdxPmpParser.c:1106>: [40;31mIt is not pmp-2.0, and is not supported. [0m
01-01 09:12:44.072 174-1349/? E/CdxOggParser: <CdxOggParser.c:2253>: [40;31mIt is not ogg version 0. [0m
01-01 09:12:44.072 174-1349/? D/CdxM3u9Parser: <CdxM3u9Parser.c:728>: M3u9ParserProbe
01-01 09:12:44.072 174-1349/? D/CdxM3u9Parser: <CdxM3u9Parser.c:735>: M3u9Probe = 0
01-01 09:12:44.072 174-1349/? D/CdxPlaylistParser: <CdxPlaylistParser.c:694>: PlaylistParserProbe
01-01 09:12:44.072 174-1349/? D/CdxPlaylistParser: <CdxPlaylistParser.c:702>: PlaylistParserProbe = 0
01-01 09:12:44.093 174-1349/? W/CdxMpgParser: <CdxMpgParser.c:840>: error: can't find mpg_pack_header_startCode 0x000001BA,B3,B8 in probe_data
01-01 09:12:44.094 174-1349/? E/CdxApeParser: <CdxApeParser.c:613>: [40;31mApe Probe Failed [0m
01-01 09:12:44.094 174-1349/? E/awplayer: <CdxFlacParse.c:980>: [40;31mFlac probe failed. [0m
01-01 09:12:44.094 174-1349/? E/awplayer: <CdxAmrParser.c:340>: [40;31mamr probe failed. [0m
01-01 09:12:44.094 174-1349/? E/CdxAtracParser: <CdxAtracParser.c:456>: [40;31mAtrac Probe Failed [0m
01-01 09:12:44.094 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.094 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.094 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.094 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.094 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.094 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.094 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.094 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.094 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.094 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.094 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.094 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.094 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.094 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.094 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.094 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.094 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.094 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.095 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.095 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.095 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.095 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.095 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.095 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.095 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.095 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.095 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.095 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.095 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.095 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.095 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.095 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.095 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.095 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.095 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.095 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.095 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.095 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.095 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.095 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.096 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.096 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.096 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.096 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.096 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.096 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.096 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.096 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.096 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.096 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.096 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.096 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.096 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.096 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.096 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.096 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.096 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.096 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.096 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.096 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.096 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.097 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.097 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.097 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.097 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.097 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.097 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.097 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.097 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.097 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.097 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.097 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.097 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.097 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.097 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.097 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.097 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.097 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.097 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.097 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.097 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.097 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.097 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.098 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.098 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.098 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.098 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.098 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.098 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.098 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.098 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.098 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.098 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.098 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.098 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.098 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.098 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.098 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.098 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.098 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.098 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.098 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.098 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.098 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.098 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.099 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.099 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.099 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.099 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.099 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.099 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.099 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.099 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.099 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.099 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.099 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.099 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.099 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.099 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.099 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.099 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.099 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.099 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.099 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.099 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.099 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.099 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.099 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.099 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.099 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.100 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.100 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.100 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.100 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.100 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.100 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.100 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.100 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.110 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.110 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.110 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.111 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.111 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.111 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.111 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.111 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.111 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.111 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.111 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.111 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.111 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.111 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.111 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.111 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.111 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.111 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.111 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.111 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.111 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.111 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.111 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.111 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.111 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.111 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.111 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.112 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.112 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.112 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.112 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.112 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.112 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.112 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.112 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.112 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.112 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.112 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.112 174-1349/? E/CdxMp3Parser: <CdxMp3Parser.c:1760>: [40;31mno dice, no valid sequence of frames found. [0m
01-01 09:12:44.112 174-1349/? W/CdxMp3Parser: <CdxMp3Parser.c:1654>: giving up at offset 65536
01-01 09:12:44.112 174-1349/? E/awplayer: <CdxAacParser.c:1597>: [40;31maudio probe fail!!! [0m
01-01 09:12:44.112 174-1349/? E/awplayer: <CdxAacParser.c:1612>: [40;31maac probe failed. [0m
01-01 09:12:44.112 174-1349/? D/awplayer: <CdxParser.c:532>: Good, it's 'wav'
01-01 09:12:44.112 174-1349/? W/awplayer: <CdxWavParser.c:409>: not implement...(265)
01-01 09:12:44.112 174-1349/? D/: <CdxParser.h:355>: *********PrintMediaInfo begin*********
01-01 09:12:44.112 174-1349/? D/: <CdxParser.h:369>: fileSize = 330810, bSeekable = 1, duration = 3750, audioNum = 1, videoNum = 0, subtitleNum = 0
01-01 09:12:44.112 174-1349/? D/: <CdxParser.h:405>: ***Audio[0]*** eCodecFormat = 0xa, eSubCodecFormat = 0x1, nChannelNum = 2, nBitsPerSample = 16, nSampleRate = 22050
01-01 09:12:44.112 174-1349/? D/: <CdxParser.h:421>: *********PrintMediaInfo end*********
01-01 09:12:44.114 174-547/? D/awplayer: <awplayer.cpp:496>: prepareAsync
01-01 09:12:44.114 475-559/system_process E/MediaPlayer: Should have subtitle controller already set
01-01 09:12:44.114 475-475/system_process E/MediaPlayer: Should have subtitle controller already set
01-01 09:12:44.115 174-174/? D/awplayer: <awplayer.cpp:557>: start
01-01 09:12:44.148 174-174/? D/awplayer: <awplayer.cpp:1688>: input invalid args.
01-01 09:12:44.148 174-1355/? W/awplayer: <AudioDec_Decode.c:679>: can't open pFileBs
01-01 09:12:44.149 174-1356/? D/awplayer: <audioRenderComponent.cpp:631>: init sound device.
01-01 09:12:44.149 174-1356/? D/awplayer: <audioRenderComponent.cpp:640>: set sound devide param, sample rate = 22050, channel num = 2.
01-01 09:12:44.151 475-559/system_process D/WindowManager: ******* wifi level good ... *******
01-01 09:12:44.151 174-1355/? D/awplayer: <adecoder.c:825>: ==============================pAudioDecoder->pBsInFor->bitrate:705600
01-01 09:12:44.159 174-1356/? D/awplayer: <awplayer.cpp:3366>: **** audio info, 0, 22050, 2, 705600
01-01 09:12:44.159 174-1356/? D/awplayer: <player.cpp:2622>: first audio pts = 0
01-01 09:12:44.159 174-1356/? D/awplayer: <audioRenderComponent.cpp:753>: start sound device.
01-01 09:12:44.161 174-470/? V/audio_hw_primary: out_set_parameters: routing=2
01-01 09:12:44.161 174-470/? V/audio_hw_primary: adev->out_device is: 2, val is : 2
01-01 09:12:44.173 174-470/? V/audio_hw_primary: start_output_stream, line: 739
01-01 09:12:44.174 174-470/? V/codec_audio_pad: headset on is: 0, headphone on is: 0, speaker on is : 2
01-01 09:12:44.174 174-470/? V/codec_audio_pad: in normal mode, headset or speaker on,****LINE:112,FUNC:set_normal_path
01-01 09:12:44.174 174-470/? V/audio_hw_primary: normal mode , speaker,****LINE:664,FUNC:select_output_device
01-01 09:12:44.174 174-470/? V/audio_hw_primary: start_output_stream: card:0, port:0, rate:44100
01-01 09:12:44.174 174-470/? V/audio_hw_primary: do not use out resampler
01-01 09:12:44.320 174-1356/? W/awplayer: <player.cpp:3067>: reset the timer to 46439, time difference is -114871
01-01 09:12:45.081 658-658/? I/wpa_supplicant: wlan0: Trying to associate with 14:ae:db:51:f6:dd (SSID='sparkup' freq=2412 MHz)
01-01 09:12:45.184 475-540/system_process E/WifiConfigStore: rewrite network history for "sparkup"WPA_PSK
01-01 09:12:45.536 658-658/? I/wpa_supplicant: wlan0: Associated with 14:ae:db:51:f6:dd
01-01 09:12:45.577 658-658/? I/wpa_supplicant: wlan0: WPA: Key negotiation completed with 14:ae:db:51:f6:dd [PTK=CCMP GTK=CCMP]
01-01 09:12:45.577 658-658/? I/wpa_supplicant: wlan0: CTRL-EVENT-CONNECTED - Connection to 14:ae:db:51:f6:dd completed [id=0 id_str=]
01-01 09:12:45.584 475-540/system_process D/ConnectivityService: registerNetworkAgent NetworkAgentInfo{ ni{[type: WIFI[], state: CONNECTING/CONNECTING, reason: (unspecified), extra: "sparkup", roaming: false, failover: false, isAvailable: true, isConnectedToProvisioningNetwork: false]} network{null} lp{{InterfaceName: wlan0 LinkAddresses: [] Routes: [] DnsAddresses: [] Domains: null MTU: 0 TcpBufferSizes: 524288,1048576,2097152,262144,524288,1048576}} nc{[ Transports: WIFI Capabilities: INTERNET&NOT_RESTRICTED&TRUSTED&NOT_VPN LinkUpBandwidth>=1048576Kbps LinkDnBandwidth>=1048576Kbps]} Score{20} everValidated{false} lastValidated{false} created{false} explicitlySelected{false} }
01-01 09:12:45.584 475-540/system_process E/WifiConfigStore: saveWifiConfigBSSID Setting BSSID for "sparkup"WPA_PSK to any
01-01 09:12:45.585 475-542/system_process D/ConnectivityService: NetworkAgentInfo [WIFI () - 101] EVENT_NETWORK_INFO_CHANGED, going from null to CONNECTING
01-01 09:12:45.602 475-540/system_process E/WifiConfigStore: saveWifiConfigBSSID Setting BSSID for "sparkup"WPA_PSK to any
01-01 09:12:45.612 170-448/? D/CommandListener: Setting iface cfg
01-01 09:12:45.613 475-540/system_process E/WifiStateMachine: Start Dhcp Watchdog 2
01-01 09:12:45.954 174-1349/? E/awplayer: <CdxWavParser.c:464>: [40;31mCdxStream EOS [0m
01-01 09:12:45.954 174-1349/? W/: <demuxComponent.cpp:2457>: read data from parser return fail.
01-01 09:12:45.954 174-1349/? W/awplayer: <awplayer.cpp:2858>: eos...
01-01 09:12:45.961 1310-1310/? E/dhcpcd: timed out
01-01 09:12:46.083 475-1305/system_process D/NetUtils: dhcp_do_request failed : wlan0 (new)
01-01 09:12:46.084 475-1305/system_process E/DhcpStateMachine: DHCP failed on wlan0: Timed out waiting for DHCP to finish
01-01 09:12:46.288 475-540/system_process E/native: do suspend true
01-01 09:12:46.435 475-540/system_process E/native: do suspend false
01-01 09:12:46.478 658-658/? E/wpa_supplicant: wpa_driver_nl80211_driver_cmd: failed to issue private command: WLS_BATCHING GET
01-01 09:12:46.478 475-540/system_process E/WifiStateMachine: Unexpected BatchedScanResults :null
01-01 09:12:46.502 658-658/? E/wpa_supplicant: wpa_driver_nl80211_driver_cmd: failed to issue private command: WLS_BATCHING STOP
01-01 09:12:46.515 475-540/system_process E/WifiConfigStore: SSID temp disabled for "sparkup"WPA_PSK had autoJoinStatus=0 self added false ephemeral false
01-01 09:12:46.515 475-540/system_process E/WifiConfigStore: message=DHCP FAILURE
01-01 09:12:46.515 475-540/system_process E/WifiConfigStore: blacklisted "sparkup"WPA_PSK to 0 due to IP config failures, count=1 disableReason=0 14:ae:db:51:f6:dd ipfail=1
01-01 09:12:46.559 658-658/? I/wpa_supplicant: wlan0: CTRL-EVENT-DISCONNECTED bssid=14:ae:db:51:f6:dd reason=3 locally_generated=1
01-01 09:12:46.569 475-540/system_process E/WifiConfigStore: saveWifiConfigBSSID Setting BSSID for "sparkup"WPA_PSK to any
01-01 09:12:46.577 475-540/system_process E/native: do suspend true
01-01 09:12:46.602 170-448/? D/CommandListener: Clearing all IP addresses on wlan0
01-01 09:12:46.612 475-540/system_process E/WifiConfigStore: saveWifiConfigBSSID Setting BSSID for "sparkup"WPA_PSK to any
01-01 09:12:46.612 475-542/system_process D/ConnectivityService: NetworkAgentInfo [WIFI () - 101] EVENT_NETWORK_INFO_CHANGED, going from CONNECTING to DISCONNECTED
01-01 09:12:46.612 475-542/system_process D/ConnectivityService: NetworkAgentInfo [WIFI () - 101] got DISCONNECTED, was satisfying 0
01-01 09:12:46.633 475-542/system_process D/ConnectivityService: notifyType LOST for NetworkAgentInfo [WIFI () - 101]
01-01 09:12:46.640 475-1358/system_process D/NetworkMonitor/NetworkAgentInfo [WIFI () - 101]: DefaultState{ when=-6ms what=532487 target=com.android.internal.util.StateMachine$SmHandler }
01-01 09:12:46.640 475-1358/system_process D/NetworkMonitor/NetworkAgentInfo [WIFI () - 101]: Disconnected - quitting
01-01 09:12:46.656 475-540/system_process E/WifiStateMachine: Start Disconnecting Watchdog 2
01-01 09:12:46.656 475-540/system_process E/native: do suspend true
01-01 09:12:46.692 170-448/? D/CommandListener: Clearing all IP addresses on wlan0
01-01 09:12:46.705 475-540/system_process D/WifiNetworkAgent: NetworkAgent: NetworkAgent channel lost
01-01 09:12:46.733 1361-1361/? I/dhcpcd: version 5.5.6 starting
01-01 09:12:46.740 1361-1361/? E/dhcpcd: get_duid: Read-only file system
01-01 09:12:46.819 1361-1361/? I/dhcpcd: wlan0: broadcasting for a lease
01-01 09:12:47.828 174-1356/? D/awplayer: <awplayer.cpp:3066>: player notify eos.
01-01 09:12:48.507 174-470/? I/AudioFlinger: BUFFER TIMEOUT: remove(4097) from active list on thread 0xb54d8000
01-01 09:12:49.151 475-559/system_process D/WindowManager: ---------------- 5s delay !!! go on next !!! ----------------
01-01 09:12:50.952 174-470/? D/audio_hw_primary: out_standby
01-01 09:12:54.152 475-559/system_process D/WindowManager: ---------------- 5s delay !!! go on next !!! ----------------
01-01 09:12:59.152 475-559/system_process D/WindowManager: ---------------- 5s delay !!! go on next !!! ----------------
01-01 09:13:04.152 475-559/system_process D/WindowManager: ---------------- 5s delay !!! go on next !!! ----------------
01-01 09:13:04.481 475-491/system_process I/MediaFocusControl: AudioFocus abandonAudioFocus() from android.media.AudioManager@28c2d0bdcom.android.music.MediaPlaybackService$3@25baa6b2
01-01 09:13:04.496 475-513/system_process I/ActivityManager: Start proc 1368:com.android.musicfx/u0a8 for broadcast com.android.musicfx/.ControlPanelReceiver
01-01 09:13:04.540 475-999/system_process I/ActivityManager: Killing 991:com.android.music/u0a35 (adj 15): empty #7
01-01 09:13:04.568 1368-1382/? I/art: Debugger is no longer active
01-01 09:13:04.645 1368-1368/? V/MusicFXControlPanelReceiver: onReceive
01-01 09:13:04.645 1368-1368/? V/MusicFXControlPanelReceiver: Action: android.media.action.CLOSE_AUDIO_EFFECT_CONTROL_SESSION
01-01 09:13:04.645 1368-1368/? V/MusicFXControlPanelReceiver: Package name: com.android.music
01-01 09:13:04.645 1368-1368/? V/MusicFXControlPanelReceiver: Audio session: 8
01-01 09:13:04.647 1368-1368/? V/MusicFXControlPanelEffect: closeSession(android.app.ReceiverRestrictedContext@294da65a, com.android.music, 😎
01-01 09:13:04.650 475-905/system_process I/ActivityManager: Killing 798:com.android.printspooler/u0a43 (adj 15): empty #7
01-01 09:13:09.153 475-559/system_process D/WindowManager: ---------------- 5s delay !!! go on next !!! ----------------
Hardware : bcm9wcd5eval1_3
SDK : started with 3.3.1 and then aded 3.4.0-aws
Followed AWS_IOT getting started guide to create a sample thing and test topic.
Using the command line on my Mac, I am able to subscribe to and publish messages.
On the bcm9wcd5eval1_3 board I am able to connect to my mqtt broker, but I am unable to send messages.
I don't get any obvious errors, but I don't see anything either on my AWSIOTLogs in CloudWatch, or in the subscriber terminal
I am using the demo.aws_iot.pub_sub.publisher as my code base.
I have copied rootCa.pem, cert.perm and private_key.pm to resources/app/secure_mqtt
and made the following changes described in the publisher.c file :
#define MQTT_BROKER_ADDRESS "A23UXEXXOFKGVR.iot.us-east-1.amazonaws.com"
#define WICED_TOPIC "topic/test"
#define CLIENT_ID "clientid1"
conninfo.port_number = 8883; <-- I tried with default value of 0 as always, but got the same behavior
Using aws cli on Mac:
terminal 1 : subscriber
$ mosquitto_sub --cafile ./rootCA.pem --cert ./cert.pem --key privateKey.pem -h A23UXEXXOFKGVR.iot.us-east-1.amazonaws.com -p 8883 -q 1 -d -t "topic/test" -i "clientid1"
Client clientid1 sending CONNECT
Client clientid1 received CONNACK
Client clientid1 sending SUBSCRIBE (Mid: 1, Topic: topic/test, QoS: 1)
Client clientid1 received SUBACK
Subscribed (mid: 1): 1
terminal 2 : publisher
$ mosquitto_pub --cafile rootCA.pem --cert cert.pem --key privateKey.pem -h A23UXEXXOFKGVR.iot.us-east-1.amazonaws.com -p 8883 -t topic/test -i clientid1 -m "Hello, Dalvi"
terminal 1 : subscriber sees published message
Client clientid1 received PUBLISH (d0, q0, r0, m0, 'topic/test', ... (12 bytes))
Hello, Dalvi
Logs from CoolTerm
Starting WICED v3.4.0-AWS
Platform BCM943341WCD1 initialised
Started ThreadX v5.6
Initialising NetX_Duo v5.7_sp2
Creating Packet pools
WWD SDIO interface initialised
WLAN MAC Address : 6C:AD:F8:F0:EC:43
WLAN Firmware : wl0: Oct 13 2014 15:25:13 version 6.10.190.51 (r507746) FWID 01-60cadeb3
Joining : mySSID
Successfully joined : mySSID
Obtaining IPv4 address via DHCP
DHCP CLIENT hostname WICED IP
IPv4 network ready IP: 10.xx.xx.xx
Setting IPv6 link-local address
IPv6 network ready IP: FE80:0000:0000:0000:6EAD:F8FF:FEF0:EC43
Resolving IP address of MQTT broker
[MQTT] Connecting to broker 54.85.255.214 ...
[MQTT] Opening connection...Success
publish_callback
[MQTT] Publishing...
mqtt_app_publish test
mqtt_app_publish success
Success
No errors while publishing the message, but on terminal 1 I don't see the message being received.
Also I don't see any logs should up on AWS CloudWatch Logs
Show LessHi,
When I am trying to build the sample application in WICED SDK 3.4.0 demo.aws_iot.light_sensor_controlled_window.subscriber-BCM9WCDPLUS114, it is throwing the following error. Can anyone provide the solution?
Thanks,
Lavanya
Show LessI am able to change the setting in wifi_dct_config.h to access the internet
/* This is the default AP the device will connect to (as a client)*/
#define CLIENT_AP_SSID "xxx"
#define CLIENT_AP_PASSPHRASE "yyy"
I have created a BLE characteristic for a user to provide the ssid/passphrase from a mobile app.
What API call do I make to setup the wifi with the ssid/passphrase I received through ble ?
Sajid
Show LessI know that you describe how to measure the power consumption of the WiCED module, e.g. in (WICED™ Development System (HW User Guide) . However, it seems to me that the method described there measures the current of MCU + WiFi chip. Is there a way to measure the current consumption of the WiFi chip, e.g.; BCM943362 only?
In this AN WICED™ Development System, Powersave Application Note , you seem to have done something similar (pg.14), but I did not see where you probed on the WiCED EVB / what you did on the HW to get these measurements.
Can someone provide some pointers on what needs to be done to isolate the power consumption measurement of the WiFi chip? I need this for a comparative analysis.
Thanks for your help!
Show LessHello,
I am working on project where I required to send packet using UDP method.
I found one App in Wiced udp_transmit. But i'm not able to send my packet.
i,e .
struct packet_data{
char str[20];
int data_length;
};
struct packet{
int i;
struct packet_data data;
char c;
};
so what is the API for sending this packet over UDP??
Thanks,
Prashant
Show LessI have some questions about there two smartbridge functions:
wiced_bt_smartbridge_gatt_read_characteristic_values_using_uuid() and wiced_bt_smartbridge_gatt_read_characteristic_value()
In official document, state the two functions as follow:
1. wiced_result_t wiced_bt_smartbridge_gatt_read_characteristic_value(X, X, X, X)
/** Read Characteristic Value
*
* @param[in] socket : socket that is connected to the server to read
* Characteristic Value from
* @param[in] handle : Attribute handle of the Characteristic Value to read
* @param[in] uuid : unique identifier of the Characteristic Value to read
* @param[out] characteristic_value : pointer that will receive the Characteristic Value
*
* @return @ref wiced_result_t
2. wiced_result_t wiced_bt_smartbridge_gatt_read_characteristic_value(X, X, X)
/** Read Characteristic Value
*
* @param[in] socket : socket that is connected to the server to read
* Characteristic Value from
* @param[in] uuid : unique identifier of the Characteristic Values to read
* @param[out] characteristic_value_list : pointer that will receive the Characteristic Value list
*
* @return @ref wiced_result_t
Example:
I create a service A (0x150A) with one characteristic A1 (0x160A) in a ble device, and use smartbridge api of wiced-wifi with ble module to connect it.
I got the correct value of A1 by calling wiced_bt_smartbridge_gatt_read_characteristic_value(X, X, 160A, X). p.s. I first find the value handle of A1.
But I got the incorrect value by calling wiced_bt_smartbridge_gatt_read_characteristic_value(X, 160A, X), this function doesn't need the parameter of the value handle.
I can not differentiate these two functions because the documents of them confuse me.
Originally, I set the A1 as a notify characteristic, and use the wiced_bt_smartbridge_get_attribute_cache_by_uuid() and wiced_bt_smartbridge_get_attribute_cache_by_handle() to read the value, refer the sample code "bt_smartbridge" in SDK. Now, I want to try some other faster and intuitive methods.
Show Less