Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Hi. All

I got bcm4390 gpio pin interrupt issue. I applied the example "client2ap and push2scan " to test gpio interrupt pin in my bcm94390 project.

but the gpio interrupt pin does not work.

the both example use the function "gpio_keypad_enable". In debug I checked when the key pressed,  "gpio_keypad_enable" function

call "gpio_interrut_key_handler", but in the fucntion "gpio_interrut_key_handler" gpio_key_internal_t* key is NULL. And did not work.

I use GPIO A8 for interrupt . I want to use the function "gpio_keypad_enable".

Plz can anyone take a look at this. And GPIO PB can be used in bcm94390WCD2?

Thanks.

0 Likes
1 Reply
Anonymous
Not applicable

Hey,

You can modify the gpio.c source to try out reading and writing to GPIO.

declare this in application_start()

wiced_bool_t gpio_status;

to read the status of the pin:-

  gpio_status=wiced_gpio_input_get(WICED_GPIO_8);

to write :-

  wiced_gpio_output_high( WICED_GPIO_8 );

OR

  wiced_gpio_output_low( WICED_GPIO_8 );

Hope that helps.

Best Regards,

AB

0 Likes