cancel
Showing results for 
Search instead for 
Did you mean: 

Wi-Fi Combo

Anonymous
Not applicable

is it possible to load a program into  an stm32f4 discovery eval board using  wiced sdk?  i have project which has F4 series as it target and presently i have an stm32f407vg eval board. i was wondering whether wiced sdk support  flashing into discovery board ?. If yes can anyone explain how. i also have a J- link with me.and stm board has SWD pins out .

thanks in advance

0 Likes
1 Solution
SeyhanA_31
Employee

Hi,

You may take a look at the blog post related to SN8000 (BCM43362 radio only module) integration with STM32F4 Discovery board (STM32F407) using Olimex debugger SN8000 WiFi Module with STM Discovery Board.

STLink debugging interface also could be used as well. For STLink please use the OpenOCD library supported for the STLink debugger. I believe the openocd-0.7.0 supports the STLink debugger.

Seyhan

View solution in original post

6 Replies
MichaelF_56
Moderator
Moderator

WICED Wi-Fi?  Note that you posted this to the WICED Smart Forum (BLE with an onboard Cortex M3), so we definitely do not have the toolchain support available to program an STM discovery board. I believe on the Wi-Fi side, we were working on something related as that platform leverages the STM32.

I can move the discussion if this is the case.

seyhan gangi

0 Likes
Anonymous
Not applicable

thank you for the help and please do move the discussion  into that group.

0 Likes
MichaelF_56
Moderator
Moderator

Moved thread to the WICED Wi-Fi forum.

SeyhanA_31
Employee

Hi,

You may take a look at the blog post related to SN8000 (BCM43362 radio only module) integration with STM32F4 Discovery board (STM32F407) using Olimex debugger SN8000 WiFi Module with STM Discovery Board.

STLink debugging interface also could be used as well. For STLink please use the OpenOCD library supported for the STLink debugger. I believe the openocd-0.7.0 supports the STLink debugger.

Seyhan

user_2177781
Valued Contributor

"STLink debugging interface also could be used as well. For STLink please use the OpenOCD library supported for the STLink debugger. I believe the openocd-0.7.0 supports the STLink debugger."


Please give more information about this statement, how do I use the ST-link if I update the OpenOCD lib to ex. 0.8.0?

0 Likes
Anonymous
Not applicable

Hi,

Has anyone run wiced SDK in STM32F4 discovery board using J-link (over SWD)? Is it possible to do so?

Best Regards,

Deepa.

0 Likes