cancel
Showing results for 
Search instead for 
Did you mean: 

Wi-Fi Combo

Anonymous
Not applicable

I need the schematics for BCM943362_EVB

What I really need is access to the UART signals to connect these directly to another UART port on external hardware

I hope these are available on one of the headers - I need the pinout please

Thanks

Greg

0 Likes
2 Replies
MichaelF_56
Moderator
Moderator

The WICED based schematics we provide are located within the SDK.

Take a look at /Wiced-SDK/Doc/Schematics

0 Likes
SeyhanA_31
Employee

Hi,

Yes, schematics are available in the SDK and for specific to BCM943362,they are located in .../platforms/BCM943362WCD4/schematics directory of the of the SDK.

Setting up uart on BCM43362 EVB, perhaps this may help you, UART Setup and Uart Messages Over Webpage

Seyhan

0 Likes