Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

The WPS enrollee feature of the WICED SDK is not working in my tests. I am running the snip.enrollee code from the unmodified SDK 3.1.2 on a BCM493362WCD4 without success. The demo.appliance is not connecting either using WPS.

I tried out different Access Points and different WLAN channels:

Firtz Box 7490

Linksys E1000

snip.wps_registrar on BCM493362WCD4

Those Access Points all worked with a LG G2 mobile phone connecting using WPS Push Button execept for the snip.wps_registrar.

Alll off the tests resulted in similar output on the UART:

Starting WICED v3.1.2

Platform BCM943362WCD4 initialised

Started ThreadX v5.6

Initialising NetX_Duo v5.7_sp1

Creating Packet pools

WWD SDIO interface initialised

WLAN MAC Address : 44:39:C4:31:79:47

WLAN Firmware    : wl0: Nov  7 2014 16:03:45 version 5.90.230.12 FWID 01-d095a660

Starting WPS Enrollee in PBC mode. Press the WPS button on your AP now.

Starting WPS Enrollee

...

followed by this sequence

...

Joining 'APPSDB_LSE1000_0001'

WPS Procedure failed. Restarting with 80 seconds left

...

or the following sequence or combinations of both

...

Joining 'APPSDB_LSE1000_0001'

Joining 'APPSDB_LSE1000_0001'

...

WPS timed out

WPS enrollment was not successful



Here seems to be a similar problem:

Using WPS to connect two WICED modules

Is anybody able to run the snip successfull? What could cause the problems?

0 Likes
1 Reply
lock attach
Attachments are accessible only for community members.
Anonymous
Not applicable

Some changes were made to the WPS code as a result of adding support for Wi-Fi Direct but some necessary changes weren't properly propagated to the WPS related snip applications. Specifically the WPS authentication and encryption types now need to be added to the device details in the apps. I'll attach a patch for the enrollee and registrar snip apps which will probably need to be manually applied. The appliance app needs more work so I don't have an easy patch for that yet.

0 Likes