cancel
Showing results for 
Search instead for 
Did you mean: 

Wi-Fi Combo

Anonymous
Not applicable

When the installation is complete, the following message is displayed: "The installation of WICED-Studio is finished, but some errors occurred during the install.  Please see the installation log for details."

Where to watch this log?

After starting WICED-Studio, the "Project Explorer" window in Eclipse is empty.

What should I do?

0 Likes
1 Solution
Anonymous
Not applicable

Thanks for the help.

I found the cause of the problem!

I changed the location of the installer "D:\Products\Радио\Wi-Fi\Радиочипы и модули\Cypress (Broadcom)\WICED-Studio-6.0.1.5-IDE-Installer" to "D:\WICED-Studio-6.0.1.5-IDE-Installer".

I'm guessing that the installation process is not friendly with the Cyrillic characters in the path name to the installer.

View solution in original post

2 Replies
ShawnA_01
Employee

C:\>set

ALLUSERSPROFILE=C:\ProgramData

APPDATA=C:\Users\snal\AppData\Roaming

TEMP=C:\Users\snal\AppData\Local\Temp

TMP=C:\Users\snal\AppData\Local\Temp

C:\>cd C:\Users\snal\AppData\Local\Temp

C:\Users\snal\AppData\Local\Temp>dir *.

Volume in drive C is Windows

Volume Serial Number is D07D-146E

Directory of C:\Users\snal\AppData\Local\Temp

11/30/2017  12:33 PM    <DIR>          .

11/30/2017  12:33 PM    <DIR>          ..

.

.

.

11/20/2017  03:45 PM    <DIR>          wiced_install_log

.

.

.

C:\Users\snal\AppData\Local\Temp>cd wiced_install_log

C:\Users\snal\AppData\Local\Temp\wiced_install_log>dir

Volume in drive C is Windows

Volume Serial Number is D07D-146E

Directory of C:\Users\snal\AppData\Local\Temp\wiced_install_log

11/20/2017  03:45 PM    <DIR>          .

11/20/2017  03:45 PM    <DIR>          ..

11/20/2017  03:45 PM         2,983,486 WICED-Studio_Install_11_20_2017_15_31_32.log

11/02/2017  10:46 AM           509,009 WICED-Studio_Uninstall_11_02_2017_11_46_09.log

11/09/2017  02:24 PM           625,901 WICED-Studio_Uninstall_11_09_2017_14_24_02.log

11/20/2017  09:44 AM           625,200 WICED-Studio_Uninstall_11_20_2017_09_44_59.log

               4 File(s)      4,743,596 bytes

               2 Dir(s)  430,161,600,512 bytes free

Anonymous
Not applicable

Thanks for the help.

I found the cause of the problem!

I changed the location of the installer "D:\Products\Радио\Wi-Fi\Радиочипы и модули\Cypress (Broadcom)\WICED-Studio-6.0.1.5-IDE-Installer" to "D:\WICED-Studio-6.0.1.5-IDE-Installer".

I'm guessing that the installation process is not friendly with the Cyrillic characters in the path name to the installer.

View solution in original post