- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I have abandoned trying to use my J-link in favor of an Olimex JTAG_ARM-USB-OCD-H dongle.
I am trying to configure WICED to use it but I am still getting the OpenOCD failure at the boot-load stage.
I have loaded the requisite drivers and my device manager shows…
WICED USB JTAG Devices
Olimex OpenOCD AMR-USB-TINY-H
Olimex OpenOCD JTAG ARM USB-TINY-H (Interface 0)
I am reasonably sure that my Olimex dongle is properly wired because I can start OpenOCD as follows:
openocd -f ./interface/ftdi/olimex-arm-usb-tiny-h.cfg
-f interface/ftdi/olimex-arm-jtag-swd.cfg
-f ./target/stm32f4x.cfg <NL>
Open On-Chip Debugger 0.9.0-rc1 (2015-04-24-22:09)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
Info : FTDI SWD mode enabled
adapter speed: 2000 kHz
adapter_nsrst_delay: 100
none separate
cortex_m reset_config sysresetreq
Info : clock speed 2000 kHz
Info : SWD IDCODE 0x2ba01477
Info : stm32f4x.cpu: hardware has 6 breakpoints, 4 watchpoints
You may have noticed, I am using the SWD interface and not JTAG. I have the Olimex SWD adapter in between the dongle and the target.
In addition, I can start a PuTTY telnet session and manually interact with OpenOCD on the target board.
First questions:
- Must I start OpenOCD prior to running WICED ?
- If so is so is there a way to make WICED do that for me?
- Is there something I need to do in WICED since I am using the SWD interface?
In WICED my Make Target entry is:
MyProgram CEL_WB4343WF3SP2 JTAG=Olimex_ARM-USB-TINY-H download
Next questions:
What settings do I need in each of the debug configuration tabs?
In Main I have:
C/C++ Applictions: build/eclipse_debug/last_built.elf
Project: WICED_SDK
In the Debugger Tab I have:
<path> \WICED\WICED-SDK-3.5.2\WICED-SDK\tools\ARM_GNU\bin\Win32\arm-none-eabi-gdb.exe
Under remote target, in the JTAG device pull-down I chose OpenOCD (via pipe)
In the Startup Tab
In the checked box under Halt I have:
add-symbol-file build/eclipse_debug/last_bootloader.elf 0x8000000
This worked before I switched to the Olimex dongle and was using a Broadcom BCM Eval module prior to my target hardware.
"Load Image" is checked using project binary.
The first entry of the openocd_log.txt file after a download attempt is...
Open On-Chip Debugger 0.9.0-00029-gafd5db2-dirty (2015-05-29-18:47)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
Info : only one transport option; autoselect 'jtag'
trst_and_srst separate srst_gates_jtag trst_push_pull srst_open_drain connect_deassert_srst
adapter speed: 1000 kHz
adapter_nsrst_delay: 100
jtag_ntrst_delay: 100
Warn : target name is deprecated use: 'cortex_m'
jtag_init
Warn : Using DEPRECATED interface driver 'ft2232'
Info : Consider using the 'ftdi' interface driver, with configuration files in interface/ftdi/...
Error: unable to open ftdi device: device not found
Sorry for all the exposition but I wanted to give as much information as possible to perhaps reduce some back and forth.
Any help convincing WICED to download my compiled program into my target via the Olimex dongle will get you included in my will.
Thanks
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
William - I am having similar troubles trying to get my Olimex working. I am looking into this.
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
Hi seyhan
Thank you for the exe. I tried it and, alas, still no joy.
After the ****OpenOCD failed.... message, the openocd_log is showing:
<snip>
jtag_init
Warn : Using DEPRECATED interface driver 'ft2232'
Info : Consider using the 'ftdi' interface driver, with configuration files in interface/ftdi/...
Error: unable to open ftdi device: device not found
<snip>
The problem is with the bootloader. (build-> waf.bootloader-NoOS-CEL_WB4343WF3SP2)
If I use the PuTTY TELNET connection and download a .ELF file, it appears to transfer to the target.
Then If I force the debugger to start within WICED I can single step through the init code although I never seem to get as far as the ELF code I loaded. I get a watchdog trap instead. But my point is that I seem to be able to do everything but boot-load through WICED. Bear in mind that I am using the SWD interface as opposed to the JTAG interface.
I just have the feeling that I am just a setting or two away from success but with all these abstraction layers I just can't figure out what to set.
Over the weekend I ever tried all this at home using a fresh install just in case I set something wrong during these last 2 painful weeks.
Any thoughts on how to get the boot-loader to work?
Best regards
Bill
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
The people at CEL provided me with a programming board that seems to solve my download problems. No more Segger or Olimex. No more SWD vs JTAG. This board uses a FTDI chip similar to the Broadcom Eval module I was using. Happy Happy day!
I re-installed WICED just to undo all the stuff I was tweaking for a fresh beginning.
I have new platform files that CEL provided describing thier module and added them to the platforms folder. The CEL module is very similar to the BCM94343WWCD1 platform so porting should be simple.
I can compile download and run with no problems. But when I try to compile debug and download I have a problem when I try to start the debugger. I get an error that says.
tools/makefiles/wiced_config.mk:356: *** No application specified. Options are: waf test README.txt wwd snip demo. Stop.
make: *** No rule to make target 'build/CEL_WB4343SP2/config.mk', needed by 'main_app'. Stop.
I added some print statements in the wiced_config.mk script that shows what the variable APP is set to. When I compile if shows the name of the program. But when I debug APP is empty.
If I ignore the error, and enter the debugger, it is stating in the console in red that
No source file named apps/snip/program_name/program_name.c
This happens even with the WICED program examples such as snip.scan.
I have tried all sorts of settings based on these and other forums and quick start guides. And I swear that I had this working properly back when I was using the Broadcom eval module but even that module behaves this way now.
I am so close to getting productive again I can taste it.
Thanks for any help
Bill
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content