cancel
Showing results for 
Search instead for 
Did you mean: 

Wi-Fi Combo

Anonymous
Not applicable

Hi!

I'm running a TCP server on Wiced AP interface and there are some issues with that when wanting to have multiple of sockets at the same time. I'm using ThreadX NetX-Duo.

Wiced has a wrapper API for TCP socket listen that defaults to the STA interface:

wiced_result_t wiced_tcp_listen( wiced_tcp_socket_t* socket, uint16_t port );

This has to be modified if you want to use the AP interface. Please add a new API or add interface parameter to the existing one.

Please consider adding:

wiced_result_t wiced_tcp_listen_ap( wiced_tcp_socket_t* socket, uint16_t port );

wiced_result_t wiced_tcp_listen_ap( wiced_tcp_socket_t* socket, uint16_t port )

{

    tcp_listen_callback_t listen_callback = NULL;

    struct NX_TCP_LISTEN_STRUCT* listen_ptr;

    WICED_LINK_CHECK( socket->socket.nx_tcp_socket_ip_ptr );

    /* Check if there is already another socket listening on the port */

    listen_ptr = IP_HANDLE(WICED_AP_INTERFACE).nx_ip_tcp_active_listen_requests;

    if ( listen_ptr != NULL )

    {

        /* Search the active listen requests for this port. */

        do

        {

            /* Determine if there is another listen request for the same port. */

            if ( listen_ptr->nx_tcp_listen_port == port )

            {

                /* Do a re-listen instead of a listen */

                if ( nx_tcp_server_socket_relisten( socket->socket.nx_tcp_socket_ip_ptr, port, &socket->socket ) == NX_SUCCESS )

                {

                    return WICED_SUCCESS;

                }

                else

                {

                    return WICED_ERROR;

                }

            }

            listen_ptr = listen_ptr->nx_tcp_listen_next;

        } while ( listen_ptr != IP_HANDLE(WICED_AP_INTERFACE).nx_ip_tcp_active_listen_requests);

    }

    /* Check if this socket has an asynchronous connect callback */

    if (socket->callbacks[WICED_TCP_CONNECT_CALLBACK_INDEX] != NULL)

    {

        listen_callback = internal_tcp_listen_callback;

    }

    if (socket->socket.nx_tcp_socket_state != NX_TCP_CLOSED)

    {

        nx_tcp_server_socket_unaccept( &socket->socket );

        if ( nx_tcp_server_socket_relisten( socket->socket.nx_tcp_socket_ip_ptr, socket->socket.nx_tcp_socket_port, &socket->socket ) == NX_SUCCESS )

        {

            return WICED_SUCCESS;

        }

        else

        {

            return WICED_ERROR;

        }

    }

    else

    {

        if ( nx_tcp_server_socket_listen( socket->socket.nx_tcp_socket_ip_ptr, port, &socket->socket, WICED_DEFAULT_TCP_LISTEN_QUEUE_SIZE, listen_callback ) == NX_SUCCESS )

        {

            return WICED_SUCCESS;

        }

        else

        {

            return WICED_ERROR;

        }

    }

}

0 Likes
1 Reply
Anonymous
Not applicable

You're right, thanks for reporting this.

A separate API shouldn't be necessary though because the socket is created using the function wiced_tcp_create_socket( wiced_tcp_socket_t* socket, wiced_interface_t interface ) which is created for a particular interface. The right approach is to grab the interface info from the socket object instead of having it hardcoded as STA. We'll fix this up in the next release.

0 Likes