cancel
Showing results for 
Search instead for 
Did you mean: 

Wi-Fi Combo

Anonymous
Not applicable

Hi all,

We are working on BCM943341WCD1 EVB. The SDK 3.1.2 seems not supporting FreeRTOS-LwIP yet because the sta_ip_handle and ap_ip_handle are not initialized in wiced_network.c. Besides, there is compile errors due to conflicted declaration of wiced_ip_handle. You can see part of codes are moved from NetX and need to rewrite for LwIP.

NX_IP* wiced_ip_handle[ 3 ] =

{

    [WICED_STA_INTERFACE] = STA_IP_HANDLE,

    [WICED_AP_INTERFACE]  = AP_IP_HANDLE,

    [WICED_P2P_INTERFACE] = P2P_IP_HANDLE

};

/* Network objects */

struct netif        wiced_ip_handle[3];

We would like to know is there any available patch for FreeRTOS-LwIP?

PS: The same application built for ThreadX-NetX runs well.

BR,

Clark

0 Likes
1 Reply
Anonymous
Not applicable

Hi Clark,

Have a look at this thread: WICED 3.1.2 Fix for FreeRTOS with LwIP

Oleg

0 Likes