- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
I hit a strange wiced_tcp_create_socket hang up,
to make sure it's not the problem of my application.
I modify apps/snip/ping_powersave/ping_powersave.c to test this issue:
Add below lines to application_start(), just before the while loop to call send_ping().
WPRINT_APP_INFO(("create socket begin\r\n"));
wiced_tcp_socket_t socket;
wiced_tcp_create_socket(&socket, WICED_STA_INTERFACE);
wiced_tcp_delete_socket(&socket);
WPRINT_APP_INFO(("create socket end\r\n"));
It then hangup after print "create socket begin".
Started FreeRTOS v7.5.2
Initialising LwIP v1.4.0.rc1
WWD SoC/4390 interface initialised
WLAN MAC Address : 02:0A:F7:E3:A2:10
WLAN Firmware : wl0: Sep 1 2014 12:37:04 version 6.38.15 (TOB) (r496949)
Joining : phoenix
Successfully joined : phoenix
Obtaining IP address via DHCP
Network ready IP: 192.168.0.101
create socket begin
Can someone explain what's wrong here?
Thanks.