Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

# Environments

- WICED Version 2.3.0

- ThreadX + NetX_Duo

- BCMUSI11 Platform

- BCM43362

Hi

We are trying to use high-speed UART and SPI. The concept is that

when data come from UART or SPI, it is sent through the Wi-Fi (and vice versa).

We are now facing with a critical interrupt problem.

When there is data traffic through the Wi-Fi, If I send a lot of data through the UART,

sometimes interrupt is not called. It is very small but critical. (about 0~30 / 1,000,000 times).

# UART Condition

- baud rate: 921600 or over

- flow-control: None or RTS+CTS

- the other is not changed

# Interrupt count check method

- Add 1 to global counter variable in the usart1_irq function.

  and check it after sending.

# Things I tried (but the problem still exist)

- Changed UART interrupt priority from 57, 68 to 00.

- Removed interrupt-disable function in the stm32f2xx_platform.c and core_cmFunc.h files.

- Uncomment #define WICED_DISABLE_MCU_POWERSAVE in the wiced_defaults.h file.

Do you have any suggestion to solve this problem ?

0 Likes
4 Replies
Anonymous
Not applicable
When the UART RX interrupt isnt fired, can you check whether the data sent from your client are already in the RX buffer? If not than perhaps the UART peripheral didnt receive the data at all.
0 Likes
Anonymous
Not applicable
The data was arrived. I could know that because the arrived one and the one got from buffer was not synced.

When I get the char from the buffer, it is not the one received right before, but received several times ago.

for example... Supposing I send "ABCDE", when I sent E, I could see B or something which is sent previously.
0 Likes
Anonymous
Not applicable
reply test
0 Likes
Anonymous
Not applicable
Is it possible for you to post your test code?

The UART API relies on the interrupt to notifies the caller via a semaphore that an X number of bytes specified has been received. It does not, however, rely on the interrupt to increment the counter every byte its received.

In cases where CPU utilisation is high, X number of bytes received does not translate to X number of UART interrupt serviced. When two or more successive interrupts fired so close together, they might be serviced together at once.

In stm32f2xx_platform.c function usart1_irq(),

------------------------------------------------------------------------------------------------------------

uart_interfaces[0].rx_buffer->tail = uart_interfaces[0].rx_buffer->size - uart_mapping[0].rx_dma_stream->NDTR;

------------------------------------------------------------------------------------------------------------

The above code does not increment the circular buffer tail by one byte; rather, it adds the total number of bytes received.
0 Likes