cancel
Showing results for 
Search instead for 
Did you mean: 

Wi-Fi Combo

user_2173276
New Contributor II

Hi!

I'm using a config AP as a way to set up credentials to join a specifc AP. Just like snip/config_mode. The problem I have is that the config AP doesn't show up when I scan for Wi-Fi networks on various devices. snip/config_mode behaves the same (doesn't show up). The example snip/APSTA works which lead me to try to join a specific AP first then start the config AP and I could find and connect to the config AP. Now is it only possible to get a config AP up running when one already has a connection to an external AP? I'm using WICED 2.4.1 and Murata sn8205 module which contains a STM32F205RGT6 with a BCM43362 wifi chip.

Greatful for any help/suggestions.

//Peter

0 Likes
8 Replies