I use below API to scan forever:
wiced_bt_ble_observe(WICED_TRUE, 0, my_scan_results_cb);
In normal case, the buffer usage is:
07:12:30.059568 --- Bluetooth(Pool type: A-App, I-Internal) Buffer summary ---␍␍␊
07:12:30.001032 Pool(size,type) Available In-use Total Max-used␍␍␊
07:12:30.008032 --------------------------------------------------------␍␍␊
07:12:30.014032 00( 64, A): 16, 0, 16, 5␍␍␊
07:12:30.020032 01( 360, A): 16, 0, 16, 3␍␍␊
07:12:30.027032 02( 360, A): 6, 0, 6, 0␍␍␊
However, sometimes the scan stop working.
The buffer usage becomes:
07:15:31.027000 --- Bluetooth(Pool type: A-App, I-Internal) Buffer summary ---␍␍␊
07:15:31.034000 Pool(size,type) Available In-use Total Max-used␍␍␊
07:15:31.041000 --------------------------------------------------------␍␍␊
07:15:31.047000 00( 64, A): 16, 0, 16, 5␍␍␊
07:15:31.054000 01( 360, A): 16, 0, 16, 3␍␍␊
07:15:31.058000 02( 360, A): 6, 0, 6, 1␍
Every time the Max-used count for large buffer becomes 1, the scan stop working.
It does not report any error but just silently get no scan result.
Note, I had reported this before but don't any fix.
Just check the status in sdk-5.1, it still has such issue.
dhak
mifo
Any one can help?
mifo wrote:
Adding the IoT Apps team: rash grsr ajai mady riya anii
Hi all,
I need to know in what kind of situation the wiced_bt_ble_observe() will use large buffer.
This information is helpful to speed up reproduce and fix this issue.
As I reported above, it indeed uses large buffer.
Hi Axel,
Please try the latest SDK and let us know your observations.
Regards,
-Madhu
mady
The Changelog does not mention any *fixes* for the BT library in latest SDK.
Can you list what is exactly *fixed* for the BT library in latest SDK?
It seems with latest sdk it does not stop immediately if hit max-used=1, but still has chance to stop latter.
Not sure if below is related, just FYI.
I tried sdk-6.0.1 and sdk-6.1.0, both have chance to hit below assertion in WICED/platform/MCU/STM32F4xx/peripherals/platform_uart.c
wiced_assert( "bad argument", ( driver != NULL ) && ( data_in != NULL ) && ( expected_data_size != NULL ) && ( *expected_data_size != 0 ) );
i.e. the caller pass 0 to expected_data_size argument.
(The caller is in binary library so I cannot check it)
Madhu Lakshmipathy wrote:
Hi Axel,
Please try the latest SDK and let us know your observations.
Regards,
-Madhu
mady
Confirm the same issue still can happen in sdk-6.1.
The ble scan no longer work without any error.
The problem is *without any error* so I even cannot workaround it.
mady
I found if there are a large number of beacons around, it's possible to hit max-used count=1 then stop scan.
It's really very difficault to handle the binary library bug like this as I cannot differentiate if no
scan result means the stop no longer work or no beacon around.