Running WICED with the BCM4330

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
dawac_2123751
Level 2
Level 2
First like received First like given
[WICED-SDK-2.2.1]

I noticed that in WICED 2.2.1 the chip that is being built for is the 43362.  Were intending to use WICED with a 4330.  Will we be able to use the chip definitions for the 43362 for the 4330?  If not, where can we get them?
0 Likes
3 Replies
Anonymous
Not applicable
4330 is not supportted in the WICED SDK.

What features of 4330 do you need?
0 Likes
dawac_2123751
Level 2
Level 2
First like received First like given
Were specifically going to be using the WLAN via SDIO, but we also intend to use BLE via UART.  We intend to use all of the security features and CCX support as well. 

If WICED wont work as a solution for us, could you direct us to documentation describing the command interface to the BCM4330 (ioctls, command sequences, etc.)?
0 Likes
Anonymous
Not applicable
Broadcom does not publish command interfaces for WLAN or Bluetooth chips.

We provide a pre-tested driver.

WICED will support the 43341 in an SDK release in June.

The 43341 is an improved version of the 4330.

If you need more info, please contact Jeff Baer : jbaer @ broadcom.com
0 Likes