- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello.
I bought CYW943907AEVAL1F.
I have to connect I2C interface (I use I2C_0 : pins 23, 25 of J6)
with intelligent battery that uses SMBus.
I have to read Battery Voltage.
For read the Battery Voltage I have to write a specific "command_code" and the read two words.
The Battery I2C address is 0001 011 ,
the "command_code" for read Voltage is 0x09 in mV.
The datasheet of the intelligent Battery states that you can read Word in this way
I write this routine :
/* i2c battery */
wiced_i2c_device_t i2c_battery;
/* setup 'i2c_battery' params */
i2c_battery.port = WICED_I2C_1;
i2c_battery.speed_mode = I2C_STANDARD_SPEED_MODE;
i2c_battery.flags = I2C_DEVICE_USE_DMA;
i2c_battery.address = 0x16 >> 1; // 0001 011 Smart Battery Data Specification V1.1 December 1998
i2c_battery.address_width = I2C_ADDRESS_WIDTH_7BIT;
/* init 'i2c_battery' i2c */
status = wiced_i2c_init ( &i2c_battery );
if ( status != WICED_SUCCESS )
{
WPRINT_APP_INFO( ("wiced_i2c_init 'i2c_battery' failed, status = %d\n", status) );
return;
}
uint8_t command_code = 0x09;
/* write command_code */
wiced_result = wiced_i2c_write ( &i2c_battery, WICED_I2C_START_FLAG, (void*)&command_code, 1U );
if ( wiced_result != WICED_SUCCESS )
{
WPRINT_APP_INFO( ("[##] wiced_i2c_write failed, status = %d\n", (int)wiced_result) );
return wiced_result;
}
/* read word */
wiced_result = wiced_i2c_read ( &i2c_battery, WICED_I2C_REPEATED_START_FLAG, (void*)&word, 2U );
if ( wiced_result != WICED_SUCCESS )
{
WPRINT_APP_INFO( ("[##] wiced_i2c_read failed, status = %d\n", (int)wiced_result) );
return wiced_result;
}
The code does't work because wiced_i2c_write fails with result 4 (WICED_ERROR).
The signals that I observe with scope are ...
What I'm wrong ?
The battery responds ACK for the Write command_code ...
Solved! Go to Solution.
- Labels:
-
WICED Studio Wi-Fi Combo
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
OK, I solved the problem.
I downgrade I2C clock to I2C_LOW_SPEED_MODE.
Battery specification states max 100kHz of clock.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
In particular I don't understand why just wiced_i2c_write produces 3 clock cycles ...
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Can you do a debug build and let me know the exact point at which this is failing and from which point the WICED_ERROR is being reported?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
1. In the wiced_i2c_write API, you need to provide the WICED_I2C_STOP_FLAG as well with the WICED_I2C_START_FLAG. In the I2C protocol, the stop condition have to be issued by the master at the end of the message frame. So, your API should look something like this-
wiced_i2c_write(&i2cDevice, WICED_I2C_START_FLAG | WICED_I2C_STOP_FLAG, tx_buffer, sizeof(tx_buffer));
2. The command code that you're sending (0x09), is this the value or the offset? As seen above the tx_buffer will contain an offset and then a single value, so we need 2 bytes in the buffer. So, you should be declaring a buffer and the first element of that buffer will be the offset and the next element would be the value. You can go through this I2C write implementation for getting better picture- https://github.com/cypresssemiconductorco/CypressAcademy_WICED_WiFi101_Files/blob/master/Projects/ww...
I hope this helps!
Thanks
Aditi
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
But the datasheet of the intelligent Battery states that you have to:
1. write 0x09 byte without STOP flag
2. read two bytes (one word)
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
OK, I solved the problem.
I downgrade I2C clock to I2C_LOW_SPEED_MODE.
Battery specification states max 100kHz of clock.