Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
CoCo_1816446
Level 4
Level 4
25 replies posted 10 replies posted 5 replies posted

I understand that I am supposed to use PSoC Creator to develop the PSoC 6 functionality and WICED for the Wi-Fi + BT functionality. What I don't understand is how a project like this should be structured. How do you create a project that you can be used in PSoC Creator and WICED interchangeably?

(I am using the CY8CKIT-062)

0 Likes
1 Solution
RaktimR_11
Moderator
Moderator
Moderator
500 replies posted 250 replies posted 100 replies posted

If you want to program just PSoC 6 MCU without wireless connectivity, you can do the same through PSoC Creator. But if you want to program the wifi-bt combo chip (CYW4343W) present in the pioneer kit, you need to download the program through WICED. Currently, there is no provision for creating a project which can be used in both the IDEs interchangeably because the development platforms are not same; WICED is eclipse based, whereas PSoC Creator is not.

View solution in original post

1 Reply
RaktimR_11
Moderator
Moderator
Moderator
500 replies posted 250 replies posted 100 replies posted

If you want to program just PSoC 6 MCU without wireless connectivity, you can do the same through PSoC Creator. But if you want to program the wifi-bt combo chip (CYW4343W) present in the pioneer kit, you need to download the program through WICED. Currently, there is no provision for creating a project which can be used in both the IDEs interchangeably because the development platforms are not same; WICED is eclipse based, whereas PSoC Creator is not.