- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I've been trying to run the WiFi Direct sample application (p2p) in the WICED 2.4.0 SDK but so far without success. After building and loading the application I am unable to discover the WICED board with my smart phone and see no probe requests when I run a wireless trace. The console output looks like:
Platform BCM943362WCD4 initialised
Started ThreadX v5.5
Initialising NetX v5.6
Creating Packet pools
Starting Wiced v2.4.0
WWD SDIO interface initialised
WLAN MAC Address : 02:0A:F7:50:BF:8D
STA MAC: 00:00:00:00:00:00
The zero MAC address looks a bit odd, but I haven't touched anything that would affect it. I've successfully built and run a couple of the other sample applications (scan and ap_clients_rssi) so I know the SDK is installed properly.
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
The problem is the P2P interface must have a different MAC address than the standard STA or AP interfaces and for modules which do not have an address written into the OTP the SDK will use a randomly generated address with the link-local bit set. The P2P intitialisation reads the STA MAC address and then sets the link-local assuming it has created a unique MAC which is not true for all modules.
A quick, temporary fix is to modify the generated_mac_address.txt file and change:
"macaddr=02:0A:F7:50:BF:8D"
"\x02\x0A\xF7\x50\xBF\x8D"
to
"macaddr=00:0A:F7:50:BF:8D"
"\x00\x0A\xF7\x50\xBF\x8D"
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I think MAC address is not written into OTP of your module.
You can program it using test.mfg_test application.
Which EVB do you use? Can you ask this someone who you got the board from?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
The problem is the P2P interface must have a different MAC address than the standard STA or AP interfaces and for modules which do not have an address written into the OTP the SDK will use a randomly generated address with the link-local bit set. The P2P intitialisation reads the STA MAC address and then sets the link-local assuming it has created a unique MAC which is not true for all modules.
A quick, temporary fix is to modify the generated_mac_address.txt file and change:
"macaddr=02:0A:F7:50:BF:8D"
"\x02\x0A\xF7\x50\xBF\x8D"
to
"macaddr=00:0A:F7:50:BF:8D"
"\x00\x0A\xF7\x50\xBF\x8D"
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Thanks, that did the trick!!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
We’re using the BCM9WCD1EVAL1 eval board with the BCM943362WCD4 module.