- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I build pwm from 101 tutorial. All other programs worked, event PuTTY up to this point. Attached is error, .mk and .c.
Error
10:24:51 **** Build of configuration Default for project 43xxx_Wi-Fi ****
"C:\\Users\\Al\\Documents\\WICED-Studio-6.2\\43xxx_Wi-Fi\\make.exe" ww101.02.09_pwm-CYW94343WWCD1_EVB download
MAKEFILE MAKECMDGOALS=ww101.02.09_pwm-CYW94343WWCD1_EVB download OTA2_SUPPORT is disabled
Building Bootloader
Building Serial Flash Loader App
MAKEFILE MAKECMDGOALS=waf.sflash_write-NoOS-CYW94343WWCD1_EVB-SDIO OTA2_SUPPORT is disabled
Finished Building Bootloader
- waf.sflash_write-NoOS-CYW94343WWCD1_EVB-SDIO
----------------------------------|---------|
| Static |
Module | RAM |
----------------------------------+---------|
App | 21130 |
Host MCU-family library | 11604 |
Interrupt Vectors | 388 |
libc | 556 |
platform | 1104 |
Ring_Buffer | 40 |
SPI_Flash_Library_CYW94343WWCD1_EV| 936 |
Startup Stack & Link Script fill | 486 |
WWD | 188 |
----------------------------------+---------|
TOTAL (bytes) | 36432 |
----------------------------------|---------|
Compiling apps_ww101_02_09_pwm
Build complete
Finished Building Serial Flash Loader App
apps/ww101/02/09_pwm/09_pwm.c: In function 'application_start':
apps/ww101/02/09_pwm/09_pwm.c:11:27: error: 'PWM_PIN' undeclared (first use in this function)
wiced_pwm_init(PWM_PIN, 1000, duty_cycle);
^~~~~~~
apps/ww101/02/09_pwm/09_pwm.c:11:27: note: each undeclared identifier is reported only once for each function it appears in
tools/makefiles/wiced_elf.mk:232: recipe for target 'build/ww101.02.09_pwm-CYW94343WWCD1_EVB/Modules/apps/ww101/02/09_pwm/09_pwm.o' failed
- make.exe[1]: *** [build/ww101.02.09_pwm-CYW94343WWCD1_EVB/Modules/apps/ww101/02/09_pwm/09_pwm.o] Error 1
Makefile:351: recipe for target 'main_app' failed
make: *** [main_app] Error 2
10:24:53 Build Finished (took 2s.184ms)
09_pwm.mk
NAME := apps_ww101_02_09_pwm
$(NAME)_SOURCES := 09_pwm.c
09_pwm.c
#include "wiced.h"
void application_start( )
{
float duty_cycle = 50.0;
wiced_init( );
wiced_gpio_deinit( WICED_LED1 );
while(1)
{
wiced_pwm_init(PWM_PIN, 1000, duty_cycle);
wiced_pwm_start(PWM_PIN);
duty_cycle += 1.0;
if(duty_cycle > 100.0)
{
duty_cycle = 0.0;
}
wiced_rtos_delay_milliseconds( 10);
}
}
Solved! Go to Solution.
- Tags:
- wiced introduction
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
In the code attached I don't see the #define for PWM_PIN, not sure if you missed pasting it here.
Another point you need to take care of is the difference in the Platforms. The training is based on the CYW943907EVAL1F and you are using the CYW94343WWCD1_EVB.
The LED's are connected to WICED_GPIO_11 & WICED_GPIO_26. Both these pins have support for PWM and can be initialized as WICED_PWM_1 & WICED_PWM_2.
Instead of using PWM_PIN, you could directly use WICED_PWM_1 or WICED_PWM_2.
Winston
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
PWM_PIN is not a predefined macro. Please place the below line after #include "wiced.h",
#define PWM_PIN WICED_PWM_n
Replace 'n' with the PWM number you want to use.
Ex: WICED_PWM_4
Regards,
Yeshwanth
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
In the code attached I don't see the #define for PWM_PIN, not sure if you missed pasting it here.
Another point you need to take care of is the difference in the Platforms. The training is based on the CYW943907EVAL1F and you are using the CYW94343WWCD1_EVB.
The LED's are connected to WICED_GPIO_11 & WICED_GPIO_26. Both these pins have support for PWM and can be initialized as WICED_PWM_1 & WICED_PWM_2.
Instead of using PWM_PIN, you could directly use WICED_PWM_1 or WICED_PWM_2.
Winston