cancel
Showing results for 
Search instead for 
Did you mean: 

Wi-Fi Combo

Anonymous
Not applicable

I've tried to create two http server instances - one for the config interface followed by another http server for the STA interface.

The STA interface' http server never worked.. when digging into the http_server codebase, I can use that it's being implemented as if only one instance is expected to be used at a time.

My question is - am I using the http_server incorrectly, or should I just re-implement the http server based on the SDK as a (great) starting point ?

Tsachi

0 Likes
1 Reply