cancel
Showing results for 
Search instead for 
Did you mean: 

Wi-Fi Combo

AnYe_1301376
New Contributor

We are currently in the design phase of a product and the WICED sdk looks like it can do the job we require.

My requirements:

wifi

blueotooth

OTA

nfc

FM radio would be great..

and embedded MCU as well...

Anyone suggest a module that will provide the above?

Have been trying to get datasheet from Murata but we get no reply

My other options are using nrf nordic bluetooth chip, esp8266 wifi, nfc module and MCU?

Anthony

0 Likes
1 Solution
DiBa_1995216
New Contributor II

The ISM43340-M4G-L44-10CF has many of the features you listed:

1.     2.4 and 5 GHz WiFi

2.     BT/BLE

3.     Microcontroller on the module - STM32F405

4.     FM is not available.

5.     NFC is no longer supported.

6.     2MB of FLASH on the module for supporting OTA.

7.     Dual Band Chip Antenna

8     FCC/IC/CE Certification

Data sheet:  http://www.inventeksys.com/wp-content/uploads/ISM4334x_M4G_L44_Functional_Spec.pdf

View solution in original post

5 Replies
MichaelF_56
Moderator
Moderator

Inventek Systems​ has three 43341 based modules that cover a majority of these requirements (I'm not sure if they have enabled FM though).

dickb​ or als@inventeksys.com​ from Inventek can help.

0 Likes
AnYe_1301376
New Contributor

can you confirm if the FM radio is exposed?

0 Likes
MichaelF_56
Moderator
Moderator

Please reach out to Inventek through one of our regional franchised Distributors

The two users at Inventek I added above may also be able to answer.

0 Likes
Anonymous
Not applicable

The FM is not exposed.

DiBa_1995216
New Contributor II

The ISM43340-M4G-L44-10CF has many of the features you listed:

1.     2.4 and 5 GHz WiFi

2.     BT/BLE

3.     Microcontroller on the module - STM32F405

4.     FM is not available.

5.     NFC is no longer supported.

6.     2MB of FLASH on the module for supporting OTA.

7.     Dual Band Chip Antenna

8     FCC/IC/CE Certification

Data sheet:  http://www.inventeksys.com/wp-content/uploads/ISM4334x_M4G_L44_Functional_Spec.pdf

View solution in original post