cancel
Showing results for 
Search instead for 
Did you mean: 

Wi-Fi Combo

Anonymous
Not applicable

Hi,

What's the maximum number BLE connections possible when using SDK 3.3.1+ on a BCM43340 or BCM4343W?  Is it possible to connect to more than one central at a time?

0 Likes
1 Solution
Anonymous
Not applicable

Hello andrew997

The Max # of simultaneous BLE connection depends on the hardware memory availability. I believe for BCM4343W it is somewhere between 4-5 Connections.

Also you can not connect central to another central, to make a connection you will have to configure the other broad to be peripheral.

I hope this helps,

Rj

View solution in original post

0 Likes
2 Replies
MichaelF_56
Moderator
Moderator

Adding jaeyoung vik86

0 Likes
Anonymous
Not applicable

Hello andrew997

The Max # of simultaneous BLE connection depends on the hardware memory availability. I believe for BCM4343W it is somewhere between 4-5 Connections.

Also you can not connect central to another central, to make a connection you will have to configure the other broad to be peripheral.

I hope this helps,

Rj

View solution in original post

0 Likes