cancel
Showing results for 
Search instead for 
Did you mean: 

Wi-Fi Combo

MaGr_2160016
New Contributor II

After a "make clean", building the ota_fr sample application, or for that matter any application with target "download_apps", results in a crash of the make. Host is Linux kubuntu 64-bit. Running as root or for the BCM943362WCD4 target results in the same crash.

Showing below the last few output lines of the command:

WICED-SDK-3.1.2$ ./make snip.ota_fr-BCMUSI14  JTAG=Olimex_ARM-USB-TINY-H VERBOSE=1 download  download_apps run

....

,...

Making snip_ota_fr-BCMUSI14.elf

"./tools/ARM_GNU/bin/Linux64/arm-none-eabi-g++" --static -Wl,-static -Wl,--warn-common -o  build/snip_ota_fr-BCMUSI14/binary/snip_ota_fr-BCMUSI14.elf @build/snip_ota_fr-BCMUSI14/binary/link.opts

"./tools/common/Linux64/echo"

"/usr/bin/perl" ./tools/mapfile_parser/map_parse_gcc.pl -a build/snip_ota_fr-BCMUSI14/binary/snip_ota_fr-BCMUSI14.map > build/snip_ota_fr-BCMUSI14/binary/snip_ota_fr-BCMUSI14_map.csv

"./tools/ARM_GNU/bin/Linux64/arm-none-eabi-strip" -o build/snip_ota_fr-BCMUSI14/binary/snip_ota_fr-BCMUSI14.stripped.elf  build/snip_ota_fr-BCMUSI14/binary/snip_ota_fr-BCMUSI14.elf

"/usr/bin/perl" ./tools/mapfile_parser/map_parse_gcc.pl build/snip_ota_fr-BCMUSI14/binary/snip_ota_fr-BCMUSI14.map

echo Making snip_ota_fr-BCMUSI14.bin

Making snip_ota_fr-BCMUSI14.bin

"./tools/ARM_GNU/bin/Linux64/arm-none-eabi-objcopy" -O binary -R .eh_frame -R .init -R .fini -R .comment -R .ARM.attributes build/snip_ota_fr-BCMUSI14/binary/snip_ota_fr-BCMUSI14.stripped.elf build/snip_ota_fr-BCMUSI14/binary/snip_ota_fr-BCMUSI14.bin

snip_ota_fr-BCMUSI14

----------------------------------|---------|---------|

                                  |         |  Static |

              Module              |  Flash  |   RAM   |

----------------------------------+---------+---------|

App                               |     293 |       0 |

base64                            |     518 |       0 |

DHCP_Server                       |    1510 |     132 |

DNS                               |      64 |      44 |

Host MCU-family library           |   14411 |    2484 |

Interrupt Vectors                 |     424 |       0 |

libc                              |   33976 |    3136 |

Networking                        |    3658 |   14318 |

NetX                              |   54658 |     536 |

NetX-Duo - Interfaces & Stacks    |       0 |      12 |

OTA_Server                        |    8239 |     676 |

Packet Buffers                    |       0 |   23142 |

platform                          |    1300 |     168 |

RAM Initialisation                |    2416 |       0 |

resources                         |      16 |       0 |

Ring_Buffer                       |      92 |       0 |

SPI_Flash_Library_BCMUSI14        |     636 |       0 |

Startup Stack & Link Script fill  |      22 |       4 |

Supplicant - BESL                 |   89988 |     516 |

ThreadX                           |    9168 |     396 |

Wi-Fi Firmware                    |  213212 |       0 |

WICED                             |    2843 |     820 |

WWD                               |   13416 |    1112 |

----------------------------------+---------+---------|

TOTAL (bytes)                     |  448444 |   47496 |

----------------------------------|---------|---------|

"./tools/common/Linux64/mkdir" -p  build/eclipse_debug/

echo Downloading Bootloader ...

Downloading Bootloader ...

"./tools/OpenOCD/Linux64/openocd-all-brcm-libftdi" -f ./tools/OpenOCD/Olimex_ARM-USB-TINY-H.cfg -f ./tools/OpenOCD/stm32f2x.cfg -f ./tools/OpenOCD/stm32f2x-flash-app.cfg -c "verify_image_checksum build/waf_bootloader-NoOS-NoNS-BCMUSI14-SDIO/binary/waf_bootloader-NoOS-NoNS-BCMUSI14-SDIO.stripped.elf" -c shutdown >> build/openocd_log.txt 2>&1 && echo No changes detected && "./tools/common/Linux64/echo" || "./tools/OpenOCD/Linux64/openocd-all-brcm-libftdi" -f ./tools/OpenOCD/Olimex_ARM-USB-TINY-H.cfg -f ./tools/OpenOCD/stm32f2x.cfg -f ./tools/OpenOCD/stm32f2x-flash-app.cfg -c "flash write_image erase build/waf_bootloader-NoOS-NoNS-BCMUSI14-SDIO/binary/waf_bootloader-NoOS-NoNS-BCMUSI14-SDIO.stripped.elf" -c shutdown >> build/openocd_log.txt 2>&1 && echo Download complete && "./tools/common/Linux64/echo" || echo "**** OpenOCD failed - ensure you have installed the driver from the drivers directory, and that the debugger is not running **** In Linux this may be due to USB access permissions. In a virtual machine it may be due to USB passthrough settings. Check in the task list that another OpenOCD process is not running. Check that you have the correct target and JTAG device plugged in. ****"

Segmentation fault (core dumped)

make: *** [main_app] Error 139


marco@kubuntu:~/fogsense/WICED-SDK-3.1.2$ file core

core: ELF 64-bit LSB core file x86-64, version 1 (SYSV), SVR4-style, from './tools/common/Linux64/make -r -j4 -f ./tools/makefiles/wiced_elf.mk snip/ota_f'


Please advise.

Thanks,

-Marco G.

0 Likes
1 Solution
Anonymous
Not applicable

Have a look at http://community.broadcom.com/thread/4456?sr=stream&ru=17953

and see if the uploaded make file solves your problem.

View solution in original post

0 Likes
5 Replies
JaeyoungY_71
Employee

Hi Marco,

Are you able to make other apps with "download run" just fine? Or is it just the "download_app" that is the problem?


We tried the snip.ota_fr app with JTAG=Olimex_ARM-USB-TINY-H on a BCM43362WCD1 with "download download_apps run", the process went fine through Windows. Could you try the following to ensure that the drivers are installer correctly?

Setup WICED USB J-TAG connection


a. For Ubuntu 12.04 and 14.04:

Create the /etc/udev/rules.d/70-wiced-JTAG.rules file as follow:

    sudo gedit /etc/udev/rules.d/70-wiced-JTAG.rules

Set the content of the file as following:

# udev rules file for WICED USB JTAG interface, to allow use by non super-users

SUBSYSTEM=="usb", ATTR{idVendor}=="0a5c", ATTR{idProduct}=="43fa", GROUP="hwlab", MODE="0666"

b. Set the serial port:

sudo modprobe ftdi_sio vendor=0x0a5c product=0x43fa


Above line could be inserted into the ~/.bashrc to load FTDI driver at startup.

Thanks,

Jaeyoung

0 Likes
MaGr_2160016
New Contributor II

Hi Jaeyoung,

I can definitely complete the build and download any application with "download run". The problem is when I use "download_apps". I have showed the ota_fr example just because is the one in the SDK with the "download_apps" make option.

Regarding the setup:

marco@kubuntu:~/fogsense/WICED-SDK-3.1.2$ more /etc/udev/rules.d/99-openocd.rules

SUBSYSTEM!="usb"

# Olimex ARM-USB-OCD

ATTRS{idVendor}=="15ba", ATTRS{idProduct}=="0003", MODE="664", GROUP="plugdev"

# Olimex ARM-USB-OCD-TINY

ATTRS{idVendor}=="15ba", ATTRS{idProduct}=="0004", MODE="664", GROUP="plugdev"

# Olimex ARM-JTAG-EW

ATTRS{idVendor}=="15ba", ATTRS{idProduct}=="001e", MODE="664", GROUP="plugdev"

# Olimex ARM-USB-OCD-TINY-H

ATTRS{idVendor}=="15ba", ATTRS{idProduct}=="002a", MODE="666", GROUP="plugdev"

# Olimex ARM-USB-OCD-H

ATTRS{idVendor}=="15ba", ATTRS{idProduct}=="002b", MODE="666", GROUP="plugdev"


Please notice that the "tools/common/Linux64/make' binary crashes. I don't get ftdi or usb errors.


Thanks,


-Marco G.

0 Likes
MaGr_2160016
New Contributor II

I have the same behavior under Mac OS host (Yosemite).

Marco-MacBook-Pro-2:WICED-SDK-3.1.2 marco$  ./make snip.ota_fr-BCMUSI14  JTAG=Olimex_ARM-USB-TINY-H VERBOSE=1 download  download_apps run

....

....

"./tools/common/OSX/mkdir" -p  build/eclipse_debug/

"./tools/common/OSX/echo" Downloading Bootloader ...

Downloading Bootloader ...

"./tools/OpenOCD/OSX/openocd-all-brcm-libftdi" -f ./tools/OpenOCD/Olimex_ARM-USB-TINY-H.cfg -f ./tools/OpenOCD/stm32f2x.cfg -f ./tools/OpenOCD/stm32f2x-flash-app.cfg -c "verify_image_checksum build/waf_bootloader-NoOS-NoNS-BCMUSI14-SDIO/binary/waf_bootloader-NoOS-NoNS-BCMUSI14-SDIO.stripped.elf" -c shutdown >> build/openocd_log.txt 2>&1 && "./tools/common/OSX/echo" No changes detected && "./tools/common/OSX/echo" || "./tools/OpenOCD/OSX/openocd-all-brcm-libftdi" -f ./tools/OpenOCD/Olimex_ARM-USB-TINY-H.cfg -f ./tools/OpenOCD/stm32f2x.cfg -f ./tools/OpenOCD/stm32f2x-flash-app.cfg -c "flash write_image erase build/waf_bootloader-NoOS-NoNS-BCMUSI14-SDIO/binary/waf_bootloader-NoOS-NoNS-BCMUSI14-SDIO.stripped.elf" -c shutdown >> build/openocd_log.txt 2>&1 && "./tools/common/OSX/echo" Download complete && "./tools/common/OSX/echo" || "./tools/common/OSX/echo" "**** OpenOCD failed - ensure you have installed the driver from the drivers directory, and that the debugger is not running **** In Linux this may be due to USB access permissions. In a virtual machine it may be due to USB passthrough settings. Check in the task list that another OpenOCD process is not running. Check that you have the correct target and JTAG device plugged in. ****"

make: *** [main_app] Segmentation fault: 11


-Marco G.

0 Likes
Anonymous
Not applicable

Have a look at http://community.broadcom.com/thread/4456?sr=stream&ru=17953

and see if the uploaded make file solves your problem.

View solution in original post

0 Likes
MaGr_2160016
New Contributor II

Yes, it does.

Marco G.

0 Likes