- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
I'm using WICED SDK 4.0.1 and using the MQTT library.
I found a small problem on QOS1.
Here's what i do :
- Publish something every 30s
- Keepalive of 10s
Both start when i receive a CONNACK.
After a while, we have this kind of event :
PING
PUBLISH packet 1
PINGRES => rePUBLISH packet 1 because still in the queue
PUBACK from packet 1
PUBACK from packet 1
and all of that in a few millisecond
Thing is, when you receive two puback from the same packet, you end up here :
if ( mqtt_session_remove_item( MQTT_PACKET_TYPE_PUBLISH, puback_args->packet_id, conn->session ) != WICED_SUCCESS ){
WPRINT_LIB_ERROR( ("[MQTT] puback %d not in session queue.\n ", puback_args->packet_id) );
}
So it can't continue. Changing to this avoid the problem, but is not solving the root cause i believe :
if ( mqtt_session_remove_item( MQTT_PACKET_TYPE_PUBLISH, puback_args->packet_id, conn->session ) != WICED_SUCCESS ){
WPRINT_APP_INFO(("[MQTT] Puback not in session\r\n"));
return WICED_ERROR;
}
I think there some room for improvement on that, because i believe QOS1 might lead to multiple PUBACK and currently in the library, it is considered as an error
Maybe in a next version of the MQTT library ?
Regards
vtunr
- Tags:
- mqtt
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Yes, I found the same issue even in the WICED SDK 6.0.