- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
- Labels:
-
SPI
- Tags:
- aware
- customers
- details
- fill
- frank
- importance
- kinetis
- mcus
- officially
- recently
- series
- shown
- shows
- significant
- support
- supported
- wiced
- wifi
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
K60 support was in 2.3.1.We are currently working on adding support for a broadcom designed WICED module with a K60.The original platform was based on a hacked up Freescale tower board.That is excellent news Jason!! I was not fully aware of that...Thanks Frank
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I am using a seperate tool (CodeWarrior Flash Programmer) to program the K60 MCU on the TWRK60D100M board
There appears to be an issue with the ELF file generated. On examining the ELF file I note the MCUs flash is erased and programmed from an offset of 8000 onwards, ie. the Vector table,etc at 0x00000 is not getting programmed?!
For comparison and analysis I have attached the following files:
snip_ping_webserver-TWRK60D100M.elf
hello_world.elf (to illustrate expected Cortex-M4 / K60 flash programming)
snip.ping_webserver-TWRK60D100M_console_log.txt
It appears additional programming of the region from 0x00000 to 0x08000 is required?
Procedure used to build ELF file was to run snip.ping_webserver-TWRK60D100M
WICED SDK version is 2.4.0
I have attached the console output from this build
Any help / insights in this regard would be welcome... 🙂
Thanks
Peter Fenn
PS: When can we expect support for mentioned "Broadcom-designed WICED module with a K60" ?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Ok, have figured-out the flash programming issue: Not obvious from the documentation but BOOTLOADER and DCT elf files needed to be separately programmed to the K60 MCU's flash memory.
ie.
0x00000 waf_bootloader-NoOS-NoNS-TWRK60D100M-SPI.elf
0x04000 DCT.elf
0x08000 snip_ping_webserver-TWRK60D100M.elf
The app now gets as far as SPI interface initialization according to my console screen:
Platform TWRK60D100M initialised
Started ThreadX v5.5
Initialising NetX v5.6
Creating Packet pools
Starting Wiced v2.4.0
WWD SPI interface initialised
Now checking network settings,etc...
Peter