- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi guys,
I would like to keep web content (.html, .js) of the web server on external flash in a filesystem.
How do I do it?
I have tried to comment the following line in the BCM943362WCD4.mk file:
INTERNAL_MEMORY_RESOURCES = $(ALL_RESOURCES)
Once built, resources content appear to be in RESOURCE_IN_FILESYSTEM:
const resource_hnd_t resources_apps_DIR_appliance_DIR_top_web_page_top_html = { RESOURCE_IN_FILESYSTEM, 785, { .fs = { 0, "top_web_page_top.html" }}};
Also wifi_firmware is RESOURCE_IN_FILESYSTEM.
However the device cannot join Wi-Fi network after that.
Not sure how to do it correctly.
I would appreciate any help on this.
Oleg
- Labels:
-
Memory
-
SDK 2.4.1
-
SDK 3.x
-
Web Services
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
there are multiple ways to achieve your target. As a start let me point out that there are two file systems in WICED 3.1.2.
- A simple read write file system (which is called multi application file system). This can take up to 7 files and should usually be used for applications and configuration files
- read only resources file system, this as the name implies is more for read only resources.
- if your web content are static and don't need to change, they can be put in the resources file system.
This is already done in BCM943362WCD4_ext platform. so rather than building for BCM943362WCD4, build for BCM943362WCD4_ext. This will put all your resources in the filesystem (it is basically doing the same thing you did plus some extra minor modifications to download the file system to external serial flash)
- if your files are dynamic you can use the mutli application read/write APIs to write these files, however pay attention to the number of files and the durability of your serial flash. for more details on this have a look at Apps/snip/ota_fr.
Regards,
Bassem
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Bassem,
Thanks for your response.
Please could you clarify about BCM943362WCD4_ext platform. It is neither in SDK 3.1.2 nor in SDK 2.4.1. Where can I find it?
Basically when I try to make a target: "snip.ota_fr-BCM943362WCD4_ext download download_apps run"
I get error: "tools/makefiles/wiced_config.mk:193: *** Unknown component: BCM943362WCD4_ext."
Many thanks.
Oleg
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
I just realized that the BCM943362WCD4_ext is not released, its part of the development only. However I'll create to a patch for you with the platform and send it to you.
Sorry for the confusion and late reply.
Regards,
Bassem
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi Bassem,
Just wondering about the progress with BCM943362WCD4_ext platform. Can it be shared yet?
Many thanks,
Oleg
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Dear Bassem,
I would like to have the BCM943362WCD4_ext platform file.
Would you send a copy to me !?
--
Thanks in advance,
Jone
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
WiConnect firmware, which is based on WICED, solves all your interactive web issues and lots more in no time flat so you can spend your valuable time focussing on your application, rather than tearing your hair out over mundane low-level wireless/networking/security issues. Think of WiConnect as WICED-on-steroids.
The latest 2.1 release includes a mobile responsive web application that talks to the WiConnect (secure) webserver via a RESTful API &/or websockets. Use the REST API to send/receive data to the serial interface, read ADC values, control GPIOs or read & write files to a bulk serial flash up to 128MB. To help you develop web apps, the WiConnect Javascript API is easily embedded into your 100% customizable web pages that are stored on the WiConnect file system.
Want to upload/download files? No problem. Just drag those files right onto your module with a mouse using the web app that comes free with WiConnect. We provide full source and a JS build system for the web app too.
More info about the core WiConnect API is available at http://wiconnect.ack.me
Info about the HTTP(S) webserver and REST API is at WiConnect - HTTP Server with RESTful API
If you need help with other features, there's loads of WiConnect Application examples too.
jc
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Bassem,
Got it!
And try it on BC943362WCD4 EVB!
It work except there are some files have to modify base on SDK 3.1.2.
--
Thanks
Jone
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi jone,
I am also working on SDK 3.1.2 and wanted to store data on external flash using SPI.
Will you please tell me what are changes or modification needed to be done in SDK 3.1.2 .
Thanking You,
Hinesh
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hinesh,
Just add "BCM943362WCD4_ext" folder into "Wiced-SDK/platforms" folder and run:
"snip.ota_fr-BCM943362WCD4_ext download download_apps run" for example.
Also have a look at this thread:
Patch to put firmware on external flash
All done by Bassem. Thanks to him.
Oleg