Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Wi-Fi Combo Forum Discussions

pelec_4022956
Level 1
Level 1

Hi,

Are there any WiFi+BT combo modules meeting following specification:

- WiFi, BT and BLE

- module should have its own MCU

- external antenna (i.e. module itself should only have a pad, which would be connected to antenna on our main board)

- Bluetooth profile HFP AG (Audio Gateway)

- (Bluetooth profile AD2P)

- I2S interface (for audio)

- UART interface (for communication between module and main CPU of the host system)

Best regards,

Pekka

0 Likes
1 Solution
SheetalJ
Moderator
Moderator 750 replies posted 500 likes received 500 replies posted
Moderator

Hi Pekka,

CYW943907WAE3 chip supports A2DP, HFP profile. Both the 43907 and 20706 have their I2S pins directly connected to the codec. This can be one of the options you are looking for.

FYI, CYW43438/CYW4343W supports A2DP, HFP is not supported. PCM is used for audio interface, not I2S.

CYW43012 supports A2DP (source) but uses UART transmission.

View solution in original post

3 Replies
SheetalJ
Moderator
Moderator 750 replies posted 500 likes received 500 replies posted
Moderator

Hi Pekka,

CYW943907WAE3 chip supports A2DP, HFP profile. Both the 43907 and 20706 have their I2S pins directly connected to the codec. This can be one of the options you are looking for.

FYI, CYW43438/CYW4343W supports A2DP, HFP is not supported. PCM is used for audio interface, not I2S.

CYW43012 supports A2DP (source) but uses UART transmission.

pelec_4022956
Level 1
Level 1

Thanks Sheetalj_96,

From where I can find information about CYW943907WAE3 chip? Seems that there is a WiFi device CYW43907 and BT device CYW20706. There is also an Evaluation kit CYW943907, but I can not find something called CYW943907WAE3.

Best regards,

Pekka

0 Likes
MichaelF_56
Moderator
Moderator 250 sign-ins 25 comments on blog 10 comments on blog
Moderator

The CYW943907WAE3 was never released to the broad market, so someone from the local/Regional Cypress Sales team would need to obtain one of these for you.

0 Likes