cancel
Showing results for 
Search instead for 
Did you mean: 

Wi-Fi Combo

AkNu_2072836
New Contributor II

We have two problems occurring.

  • case 1
    • Installing WICED Studio takes a long time to install on a specific PC.
      (It took more than an hour.)
  • case 2
    • Full build takes more than 2 hours to complete.

I tried it on some PCs and found that Windows10(1709)

and Core i5-8500 (Coffee Lake-S), It appears to be occurring in combination.

Does anyone know how to solve problems with this combination?

※ Attached file is the result of trial.

0 Likes
1 Solution
RaktimR_11
Moderator
Moderator

The numbers that you are mentioning seems really high to me. I am using a WIN 10 build 1607, 2.30 GHz, 8 GB RAM PC and has never faced this kind of issue or have not heard others face this kind of issue as well. You can try debugging through the installation log located in your Appdata folder but it seems to me a machine specific issue to me which have been previously unknown to us.

View solution in original post

2 Replies
RaktimR_11
Moderator
Moderator

The numbers that you are mentioning seems really high to me. I am using a WIN 10 build 1607, 2.30 GHz, 8 GB RAM PC and has never faced this kind of issue or have not heard others face this kind of issue as well. You can try debugging through the installation log located in your Appdata folder but it seems to me a machine specific issue to me which have been previously unknown to us.

View solution in original post

AkNu_2072836
New Contributor II

> a machine specific issue

I was thinking so too.

Fortunately, we have other machine which works well and I'll use it.

For a machine specific issue, I'll try looking for another way to avoid it.

Thanks.

0 Likes