cancel
Showing results for 
Search instead for 
Did you mean: 

Wi-Fi Combo

Anonymous
Not applicable

Hi All,

When implement

void ble_scan_results_cb( wiced_bt_ble_scan_results_t* p_scan_result, uint8_t* p_adv_data )

for API wiced_bt_ble_observe( WICED_TRUE, 30, ble_scan_results_cb )

The p_adv_data carries full packet of data ( without size info, please add size info in API to make life easier)

If p_scan_result->ble_evt_type is BTM_BLE_EVT_CONNECTABLE_ADVERTISEMENT, p_adv_data carries advertisement data, that's fine.

But if p_scan_result->ble_evt_type is BTM_BLE_EVT_SCAN_RSP (for same device), p_adv_data carries advertisement with scan response data concatenated.

Is there a boundary info to separate scan response data from the whole bunch of data ?

It's really hard to do this.

0 Likes
7 Replies
AxLi_1746341
Honored Contributor

Hi jaeyoungdkumar​,

any comment about this?

People need to know how to parse the p_adv_dta for BTM_BLE_EVT_SCAN_RSP case.

Anonymous
Not applicable

sam.linaxel.lin

Can you post the response data which you're getting for the two cases(i.e. BTM_BLE_EVT_CONNECTABLE_ADVERTISEMENT and BTM_BLE_EVT_SCAN_RSP)?

Br,
Dharam

Anonymous
Not applicable

Here is some log:

address:cc b9 7e 73 61 a4 rssi:-48 bdaddrtype:1 event_type:0

App Scan payload  -32  (17) [0201050D0953657269616C494F20424C45]

==> BTM_BLE_EVT_CONNECTABLE_ADVERTISEMENT

address:cc b9 7e 73 61 a4 rssi:-46 bdaddrtype:1 event_type:4

[App] Scan payload  -46  (39) [0201050D0953657269616C494F20424C4503030A181107F74F3A0B960541B1594D66D6010092BA]

==> BTM_BLE_EVT_SCAN_RSP

This is from same device, in BTM_BLE_EVT_CONNECTABLE_ADVERTISEMENT case

the payload is [0201050D0953657269616C494F20424C45] (17 bytes), thie is ADV data

in BTM_BLE_EVT_SCAN_RSP case

the payload becomes [0201050D0953657269616C494F20424C4503030A181107F74F3A0B960541B1594D66D6010092BA]  (34 bytes),

this is ADV data concatenated with Scan Response data.

0 Likes
PrejithP_01
Employee

Hi axel.lin

wiced_bt_ble_observe api gives you non connectable advertisements (i.e Beacons)  , The first byte of  advertisement data is length , this is as per the BT specification [volume 3 , part C : Advertisement and Scan response format ]

The structure wiced_bt_ble_scan_results_t has a field named named ble_evt_type which inturn tells you if the data received is  SCAN_RSP

Can you send me the application logs where you see ADV data and scan data being concatenated ,  most peripherals fill the same data as ADV and Scan RSP


Regards
Prejith

Anonymous
Not applicable

Hi prejith,

That's not quite true about the length.

Here is an diagram about eh advertising data

https://docs.mbed.com/docs/ble-intros/en/master/Advanced/Images/GAP/GeneralStruct.png

advertising data is a byte array which contains multiple AD structure, the first byte of AD structure only indicates length of the AD structure instead of total advertising data.

for example:

address:cc b9 7e 73 61 a4 rssi:-48 bdaddrtype:1 event_type:0

App Scan payload  -32  (17) [0201050D0953657269616C494F20424C45]

The advertising data is [0201050D0953657269616C494F20424C45] this is what p_adv_data point to.

It contains 2 AD structures:

020105

0D0953657269616C494F20424C45

The first byte 02 only indicate the first AD structure length.

To get total length of the payload (17 bytes) you need to parse traversal every AD structure and sum them up.

If the parsing or the payload is wrong, you might end up with segfault.

I think better and safer API should provide the length of the payload.

0 Likes
PrejithP_01
Employee

Hi Sam

Regarding ADV data you are right , peripherals fill different AD structures and its a variable length , to parse the advertising data you can use the below api

/**

*

* Function         wiced_bt_ble_check_advertising_data

*

*                  Parse advertising data (returned from scan results callback #wiced_bt_ble_scan_result_cback_t).

*                  Look for specified advertisement data type.

*

* @param[in]       p_adv       : pointer to advertisement data

* @param[in]       type        : advertisement data type to look for

* @param[out]      p_length    : length of advertisement data (if found)

*

* @return          pointer to start of requested advertisement data (if found). NULL if requested data type not found.

*

*/

uint8_t *wiced_bt_ble_check_advertising_data( uint8_t *p_adv, wiced_bt_ble_advert_type_t type, uint8_t *p_length);

Regarding scan response : You are right wiced stack concatenates all the active scan data and passes it to the application , however if you are interested to check any AD type you can use the above api's on the complete concatenated advertisement data

Regarding your question relating to length : Can you let us know why would you need the length , usually the scanner knows the kind of data it is expecting (for example , service UUID , name etc etc ) , and the above api should be able to help you get the same.

Regards

Prejith

Anonymous
Not applicable

Hi prejith,

For our case we relays raw payload to remote site so we may not really care about content.

With length info we can do memory copy directly without payload traversal.

Regards,

Sam

0 Likes