Anonymous
Not applicable
Mar 17, 2013
09:53 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Mar 17, 2013
09:53 PM
[WICED-SDK-2.1.1]What is the best way to minimise WICED power consumption?
Labels
- Tags:
- 1.9ma
- 170ua
- 200ua
- 32khz
- 43362
- accurate
- andor
- apply
- average
- averaged
- back
- bcm43362
- beacon
- beacons
- broadcom
- chip
- chips
- clock
- connected
- consume
- consumption
- current
- datasheet
- device
- dtim=1
- ext_sleep_clk
- forum
- http:forum.broadcom.comshowthread.php35699-should-i-connect-the-wi-fi-sleep-clock-input
- important
- info
- interval
- long
- make
- minimise
- misses
- modes
- note
- numbers
- oscillator
- post
- power
- probe
- sleep
- staying
- supplied
- sync
- times
- wakes
- wakeup
- wi-fi
1 Reply
Anonymous
Not applicable
Mar 17, 2013
10:00 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Mar 17, 2013
10:00 PM
The numbers below apply to the BCM43362 Wi-Fi chip.Other Broadcom Wi-Fi chips may consume less current and/or have other power consumption modes.From the 43362 datasheet, the average current consumption for DTIM=1 is 1.9mA.200uA of this is quiescent sleep current, 1.7mA is current used to wakeup to receive a 1ms beacon every 100ms.If the listen interval is set so that the 43362 only wakes every 10 (or 100) beacons (instead of every beacon),
- 1 second wakeup : 200uA = sleep, wakeup is averaged at 170uA
- 10 second wakeup : 200uA = sleep, wakeup is averaged at 17uA