cancel
Showing results for 
Search instead for 
Did you mean: 

Wi-Fi Combo

Anonymous
Not applicable

From WICED debug, it is appear thread[1] only,

How can I to trace or create thread[?] to debug breakpoint step run?

0 Likes
1 Reply
SeyhanA_31
Employee

Hi,

First thread is the main thread shown when the debugging starts.

If the application is started then it is suspended, all created thread will be present to be examined.

It is possible set a break point and the execution will be suspended when the break point is hit.

-Seyhan