Hello
Is there a way to flash the BCM/CYW43907 through the JLink standard tools? I tried it with these settings, but it did not succeed:
Erasing seems to work, at least I don't get an error message.
This entry was not helpful for me:
Downloading and debugging CYW43907 using Jlink Segger
We need this possibility to flash the device for the first samples in the lab and also to be prepared for end-of-line flashing.
Thank you!
Solved! Go to Solution.
Apologies for the delayed response. Please check the attached for the necessary changes to be made in WICED SDK for successfully downloading through native J-link.
In the latest WICED Studio, the native J-Link Support is added so you can bypass the driver changing procedure mentioned in the blog post and directly download through WICED SDK. Do you have any particular reason not to use WICED SDK to download?
If it's possible to use WICED SDK for downloading, you can check the updated native J-Link support in wiced_apps.mk and BCM94390x_targets.mk through which you should be able to download. The build statement to use the native J-Link should look something like this
test.console-CYW943907AEVAL1F JLINK_NATIVE=1 JLINK_PATH="../../../../Program\ Files\ \(x86\)/SEGGER/JLink_V630c/" JLINK_EXE="Jlink.exe" download run
Thank you for the reply. We tried the original drivers, but it did not work. When trying to download, it keeps telling "Unspecified error -1" and "****** Error: Could not read CP15 register.". Nevertheless, it sees the target voltage. And flashing with the OpenOCD configuration and libK works. Can you imagine what's the issue?
Here is the full log:
C:\Projekte\XYZ\xyz_tgt_wifi>43xxx_Wi-Fi\make.exe -C 43xxx_Wi-Fi tgt_wifi-XYZ_LV_MCU-debug JTAG=jlink-native JLINK_PATH="C:/Tool/SEGGER/JLink_V634a/" JLINK_EXE="JLink.exe" JLINK_DEVICE=CYW43907 JLINK_SPEED=auto JLINK_INTERFACE=JTAG JLINK_AUTO_CONNECT=1 VERBOSE=1 download run
MAKEFILE MAKECMDGOALS=tgt_wifi-XYZ_LV_MCU-debug download run OTA2_SUPPORT is disabled
make: Entering directory 'C:/Projekte/XYZ/xyz_tgt_wifi/43xxx_Wi-Fi'
./tools/common/Win32/mkdir -p build/tgt_wifi-XYZ_LV_MCU-debug/binary build/tgt_wifi-XYZ_LV_MCU-debug/modules build/tgt_wifi-XYZ_LV_MCU-debug/libraries build/tgt_wifi-XYZ_LV_MCU-debug/resources
"./tools/common/Win32/make.exe" -r -j4 -f ./tools/makefiles/wiced_elf.mk tgt_wifi-XYZ_LV_MCU-debug download run
make.exe[1]: Entering directory 'C:/Projekte/XYZ/xyz_tgt_wifi/43xxx_Wi-Fi'
echo Building Bootloader waf.bootloader-NoOS-NoNS-XYZ_LV_MCU-REV_B-SoC.43909
Building Bootloader waf.bootloader-NoOS-NoNS-XYZ_LV_MCU-REV_B-SoC.43909
"./tools/common/Win32/make.exe" -r -f ./Makefile waf.bootloader-NoOS-NoNS-XYZ_LV_MCU-REV_B-SoC.43909 -Ibuild/tgt_wifi-XYZ_LV_MCU-debug SFLASH= EXTERNAL_WICED_GLOBAL_DEFINES= SUB_BUILD=bootloader
MAKEFILE MAKECMDGOALS=waf.bootloader-NoOS-NoNS-XYZ_LV_MCU-REV_B-SoC.43909 OTA2_SUPPORT is disabled
make.exe[2]: Entering directory 'C:/Projekte/XYZ/xyz_tgt_wifi/43xxx_Wi-Fi'
./tools/common/Win32/mkdir -p build/waf.bootloader-NoOS-NoNS-XYZ_LV_MCU-REV_B-SoC.43909/binary build/waf.bootloader-NoOS-NoNS-XYZ_LV_MCU-REV_B-SoC.43909/modules build/waf.bootloader-NoOS-NoNS-XYZ_LV_MCU-REV_B-SoC.43909/libraries build/waf.bootloader-NoOS-NoNS-XYZ_LV_MCU-REV_B-SoC.43909/resources
"./tools/common/Win32/make.exe" -r -f ./tools/makefiles/wiced_elf.mk waf.bootloader-NoOS-NoNS-XYZ_LV_MCU-REV_B-SoC.43909
echo Using jlink_native and ignore sflash_write_app ...
make.exe[3]: Entering directory 'C:/Projekte/XYZ/xyz_tgt_wifi/43xxx_Wi-Fi'
"./tools/common/Win32/perl.exe" ./tools/mapfile_parser/map_parse_gcc.pl build/waf.bootloader-NoOS-NoNS-XYZ_LV_MCU-REV_B-SoC.43909/binary/waf.bootloader-NoOS-NoNS-XYZ_LV_MCU-REV_B-SoC.43909.map
waf.bootloader-NoOS-NoNS-XYZ_LV_MCU-REV_B-SoC.43909
----------------------------------|---------|---------|
| | Static |
Module | Flash | RAM |
----------------------------------+---------+---------|
App | 0 | 120 |
crc | 0 | 1060 |
Interrupt Vectors | 0 | 224 |
libc | 0 | 488 |
Other | 0 | 12878 |
platform | 0 | 290 |
RAM Initialisation | 32 | 0 |
Startup Stack & Link Script fill | 0 | 8318 |
WWD | 0 | 106 |
----------------------------------+---------+---------|
TOTAL (bytes) | 0 | 23484 |
----------------------------------|---------|---------|
make.exe[3]: Leaving directory 'C:/Projekte/XYZ/xyz_tgt_wifi/43xxx_Wi-Fi'
echo Build complete
Using jlink_native and ignore sflash_write_app ...
Build complete
make.exe[2]: Leaving directory 'C:/Projekte/XYZ/xyz_tgt_wifi/43xxx_Wi-Fi'
"./tools/common/Win32/perl.exe" ./WICED/platform/MCU/BCM4390x/make_trx.pl build/waf.bootloader-NoOS-NoNS-XYZ_LV_MCU-REV_B-SoC.43909/binary/waf.bootloader-NoOS-NoNS-XYZ_LV_MCU-REV_B-SoC.43909.elf build/waf.bootloader-NoOS-NoNS-XYZ_LV_MCU-REV_B-SoC.43909/binary/waf.bootloader-NoOS-NoNS-XYZ_LV_MCU-REV_B-SoC.43909.trx.bin
prgm hdr cnt=3
total_size = 14652, entry_point = 0x696000
Loadsegment_offset = 0xA0 segment_size = 14416, segment_pad = 0
Loadsegment_offset = 0x38F0 segment_size = 32, segment_pad = 0
Loadsegment_offset = 0x3910 segment_size = 204, segment_pad = 0
echo Finished Building Bootloader
Finished Building Bootloader
"./tools/common/Win32/echo.exe"
"./tools/common/Win32/perl.exe" ./tools/mapfile_parser/map_parse_gcc.pl build/tgt_wifi-XYZ_LV_MCU-debug/binary/tgt_wifi-XYZ_LV_MCU-debug.map
tgt_wifi-XYZ_LV_MCU-debug
----------------------------------|---------|---------|
| | Static |
Module | Flash | RAM |
----------------------------------+---------+---------|
App | 0 | 12629 |
crc | 0 | 1102 |
DHCP_Server | 0 | 3000 |
DNS | 0 | 180 |
Interrupt Vectors | 0 | 498 |
libc | 0 | 30679 |
Networking | 0 | 31378 |
NetX-Duo - Interfaces & Stacks | 0 | 16 |
NVRam | 0 | 2109 |
Other | 0 | 185570 |
Packet Buffers | 0 | 71659 |
platform | 0 | 638 |
RAM Initialisation | 32 | 0 |
resources | 0 | 32 |
Ring_Buffer | 0 | 314 |
Startup Stack & Link Script fill | 0 | 190 |
Supplicant - BESL | 0 | 176 |
ThreadX | 0 | 24928 |
TLV | 0 | 92 |
WICED | 0 | 8904 |
Wiced_RO_FS | 0 | 1016 |
WWD | 0 | 5378 |
----------------------------------+---------+---------|
TOTAL (bytes) | 0 | 380488 |
----------------------------------|---------|---------|
"./tools/common/Win32/cp.exe" -f build/tgt_wifi-XYZ_LV_MCU-debug/binary/tgt_wifi-XYZ_LV_MCU-debug.elf build/eclipse_debug/last_built.elf
echo Creating Filesystem BCM94390x_targets.mk ...
Creating Filesystem BCM94390x_targets.mk ...
"./tools/common/Win32/rm.exe" -f build/tgt_wifi-XYZ_LV_MCU-debug/resources/Staging/app.elf
echo Downloading DCT ... build/tgt_wifi-XYZ_LV_MCU-debug/DCT.bin @ SFLASH_DCT_LOC=0x00008000
echo ./tools/common/Win32/mk_wicedfs32 build/tgt_wifi-XYZ_LV_MCU-debug/filesystem.bin build/tgt_wifi-XYZ_LV_MCU-debug/resources/Staging/
Downloading DCT ... build/tgt_wifi-XYZ_LV_MCU-debug/DCT.bin @ SFLASH_DCT_LOC=0x00008000
C:\Tool\SEGGER\JLink_V634a\JLink.exe -device CYW43907 -if JTAG -speed auto -jtagconf -1,-1 -autoconnect 1 -CommanderScript jlink_commander_script.txt
./tools/common/Win32/mk_wicedfs32 build/tgt_wifi-XYZ_LV_MCU-debug/filesystem.bin build/tgt_wifi-XYZ_LV_MCU-debug/resources/Staging/
./tools/common/Win32/mk_wicedfs32 build/tgt_wifi-XYZ_LV_MCU-debug/filesystem.bin build/tgt_wifi-XYZ_LV_MCU-debug/resources/Staging/
echo Creating Filesystem Done
Creating Filesystem Done
echo Building apps lookup table
Building apps lookup table
"./tools/ARM_GNU/Win32/bin/arm-none-eabi-gcc.exe" -isystem ./tools/ARM_GNU/Win32/bin/../../include -isystem ./tools/ARM_GNU/Win32/bin/../../lib/include -isystem ./tools/ARM_GNU/Win32/bin/../../lib/include-fixed -mcpu=cortex-r4 -mthumb-interwork -mthumb -fno-builtin-memcpy -c ./WICED/platform/MCU/wiced_apps_lut.c -DFR_APP_ENTRY_COUNT=0 -DFR_APP_SECTOR_START=0 -DFR_APP_SECTOR_COUNT=0 -DFR_APP_IS_SECURE=0 -DDCT_IMAGE_ENTRY_COUNT=0 -DDCT_IMAGE_SECTOR_START=0 -DDCT_IMAGE_SECTOR_COUNT=0 -DDCT_IMAGE_IS_SECURE=0 -DOTA_APP_ENTRY_COUNT=0 -DOTA_APP_SECTOR_START=0 -DOTA_APP_SECTOR_COUNT=0 -DOTA_APP_IS_SECURE=0 -DFILESYSTEM_IMAGE_ENTRY_COUNT=1 -DFILESYSTEM_IMAGE_SECTOR_START=17
-DFILESYSTEM_IMAGE_SECTOR_COUNT=125 -DFILESYSTEM_IMAGE_IS_SECURE=0 -DWIFI_FIRMWARE_ENTRY_COUNT=0 -DWIFI_FIRMWARE_SECTOR_START=0 -DWIFI_FIRMWARE_SECTOR_COUNT=0 -DWIFI_FIRMWARE_IS_SECURE=0 -DAPP0_ENTRY_COUNT=1 -DAPP0_SECTOR_START=142 -DAPP0_SECTOR_COUNT=66 -DAPP0_IS_SECURE=0 -DAPP1_ENTRY_COUNT=0 -DAPP1_SECTOR_START=0 -DAPP1_SECTOR_COUNT=0 -DAPP1_IS_SECURE=0 -DAPP2_ENTRY_COUNT=0 -DAPP2_SECTOR_START=0 -DAPP2_SECTOR_COUNT=0 -DAPP2_IS_SECURE=0 -DWICED_USE_ETHERNET_INTERFACE -DWICED_ETHERNET_BUFFER_SIZE=1580 -DSFLASH_APPS_HEADER_LOC=0x00010000 -DPLATFORM_NO_DDR=1 -DPLATFORM_HAS_HW_CRYPTO_SUPPORT -DOTP_WORD_NUM_SHA_KEY=258 -DOTP_WORD_NUM_SHA_KEY_R=242 -DOTP_WORD_NUM_AES_KEY=282 -DOTP_WORD_NUM_AES_KEY_R=274 -DSECUREBOOT_SHA_KEY_SIZE=32 -DGSIO_I2C_REPEATED_START_NEEDS_GPIO=1 -DPLATFORM_HIB_WAKE_CTRL_FREQ_BITS_FLIPPED -DCRLF_STDIO_REPLACEMENT -DAPP_NAME=\"tgt_wifi\" -DWICED_DISABLE_CONFIG_TLS -DPLATFORM_SECURESFLASH_ENABLED=0 -DPLATFORM_SECUREDCT_ENABLED=0 -DNORMAL_IMAGE_FLASH_BASE=0x00000000 -DNORMAL_IMAGE_BOOTLOADER_START=0x00000000 -DNORMAL_IMAGE_DCT_1_AREA_BASE=0x00008000 -DNORMAL_IMAGE_DCT_2_AREA_BASE=0x0000C000 -DNORMAL_IMAGE_LUT_AREA_BASE=0x00010000 -DNORMAL_IMAGE_APPS_AREA_BASE=0x00011000 -DNORMAL_IMAGE_FS_AREA_BASE=0x00011000 -DMIN_WM8533_DB_LEVEL=-53.0 -DMAX_WM8533_DB_LEVEL=6.0 -DPLATFORM_ALP_CLOCK_RES_FIXUP=0 -DMAX_WATCHDOG_TIMEOUT_SECONDS=22 -DMAX_WAKE_FROM_SLEEP_DELAY_TICKS=500 -DPLATFORM_L1_CACHE_SHIFT=5 -DPLATFORM_SUPPORTS_LOW_POWER_MODES -DBCM43909 -DENABLE_ARM_DSP_INSTRUCTIONS -DPLAT_NOTIFY_FREE -DDCT_SFLASH_COPY_BUFFER_SIZE_ON_STACK=1024 -DUSING_WICEDFS -DNETWORK_NetX_Duo=1 -DNetX_Duo_VERSION=\"v5.10_sp3\" -DNX_INCLUDE_USER_DEFINE_FILE -D__fd_set_defined -DSYS_TIME_H_AVAILABLE -DADD_LWIP_EAPOL_SUPPORT -DNXD_EXTENDED_BSD_SOCKET_SUPPORT -DOPENSSL -DSTDC_HEADERS -Dwifi_firmware_image=resources_firmware_DIR_43909_DIR_43909B0_bin -Dwifi_firmware_clm_blob=resources_firmware_DIR_43909_DIR_43909B0_clm_blob -DWWD_DOWNLOAD_CLM_BLOB -DADD_NETX_EAPOL_SUPPORT -DNX_FRAGMENT_IMMEDIATE_ASSEMBLY -DWWD_STARTUP_DELAY=10 -DBOOTLOADER_MAGIC_NUMBER=0x4d435242 -DRTOS_ThreadX=1 -DThreadX_VERSION=\"v5.8\" -DTX_INCLUDE_USER_DEFINE_FILE -D__TARGET_ARCH_ARM=7 -D__THUMB_INTERWORK -DWICED_DISABLE_WATCHDOG -DWICED_SDK_WIFI_CONFIG_DCT_H=\"./include/default_wifi_config_dct.h\" -DWICED_SDK_BT_CONFIG_DCT_H=\"./include/default_bt_config_dct.h\" -I./WICED/platform/MCU/BCM4390x/peripherals/spi_flash/. -I./libraries/daemons/DHCP_server/. -I./libraries/utilities/ring_buffer/. -I./WICED/platform/GCC/. -I./libraries/inputs/gpio_button/. -I./libraries/utilities/crc/. -I././WICED/network/NetX_Duo/WICED/. -I././WICED/network/NetX_Duo/WWD/. -I./WICED/security/BESL/crypto_internal/micro-ecc/. -I./WICED/security/BESL/mbedtls_open/include -I./libraries/utilities/linked_list/. -I./libraries/utilities/base64/. -I./libraries/utilities/TLV/. -I./libraries/test/TraceX/. -I././WICED/platform/MCU/BCM4390x/. -I././WICED/platform/MCU/BCM4390x/.. -I././WICED/platform/MCU/BCM4390x/../../ARM_CR4 -I././WICED/platform/MCU/BCM4390x/WAF -I././WICED/platform/MCU/BCM4390x/peripherals -I././WICED/platform/MCU/BCM4390x/peripherals/include -I././WICED/platform/MCU/BCM4390x/peripherals/tlsf -I././WICED/platform/MCU/BCM4390x/./Library/drivers/spi_flash -I././WICED/platform/MCU/BCM4390x/./platforms/XYZ_LV_MCU -I././WICED/platform/MCU/BCM4390x/..//platforms/XYZ_LV_MCU/ -I././WICED/platform/MCU/BCM4390x/./WICED/platform/include -I././WICED/platform/MCU/BCM4390x/./libraries/bluetooth/include -I././WICED/platform/MCU/BCM4390x/./libraries/inputs/gpio_button -I./libraries/filesystems/wicedfs/src -I./WICED/network/NetX_Duo/ver5.10_sp3 -I./WICED/network/NetX_Duo/ver5.10_sp3/netx_bsd_layer -I./WICED/network/NetX_Duo/WICED -I./libraries/protocols/DNS/. -I././WICED/security/PostgreSQL/include -I././WICED/security/BESL/host/WICED -I././WICED/security/BESL/TLS -I././WICED/security/BESL/crypto_internal -I././WICED/security/BESL/WPS -I././WICED/security/BESL/include -I././WICED/security/BESL/P2P -I././WICED/security/BESL/crypto_internal/homekit_srp -I././WICED/security/BESL/crypto_internal/ed25519 -I././WICED/security/BESL/supplicant -I././WICED/security/BESL/DTLS -I././WICED/security/BESL/mbedtls_open/include -I././WICED/WWD/. -I././WICED/WWD/include -I././WICED/WWD/include/network -I././WICED/WWD/include/RTOS -I././WICED/WWD/internal/bus_protocols/SoC/43909 -I././WICED/WWD/internal/chips/4390x -I././WICED/WWD/../../libraries/utilities/linked_list -I././WICED/WWD/../RTOS/ThreadX/WICED -I././WICED/RTOS/ThreadX/WICED/. -I././WICED/RTOS/ThreadX/WWD/. -I././WICED/RTOS/ThreadX/WWD/CR4 -I././WICED/. -I././WICED/platform/include -I./WICED/RTOS/ThreadX/ver5.8 -I./WICED/RTOS/ThreadX/ver5.8/Cortex_R4/GCC -I./WICED/RTOS/ThreadX/WWD/CR4 -I./platforms/XYZ_LV_MCU/. -I./platforms/XYZ_LV_MCU/./board_revision/REV_B -I./WICED/WWD/internal/chips/4390x -I./libraries -I./include -DDEBUG -ggdb -O0 -Wall -fsigned-char -ffunction-sections -fdata-sections -fno-common -std=gnu11 -fdiagnostics-color -Ibuild/tgt_wifi-XYZ_LV_MCU-debug -I./. -o build/tgt_wifi-XYZ_LV_MCU-debug/apps_header.o
"./tools/ARM_GNU/Win32/bin/arm-none-eabi-g++.exe" -isystem ./tools/ARM_GNU/Win32/bin/../../include -isystem ./tools/ARM_GNU/Win32/bin/../../lib/include -isystem ./tools/ARM_GNU/Win32/bin/../../lib/include-fixed --static -Wl,-static -Wl,--warn-common -Wl,--gc-sections -Wl,--cref -mthumb -mcpu=cortex-r4 -mthumb-interwork -Wl,-A,thumb -Wl,-z,max-page-size=0x10 -Wl,-z,common-page-size=0x10 -mlittle-endian -nostartfiles -Wl,--defsym,START_STACK_SIZE=800 -Wl,--defsym,FIQ_STACK_SIZE=0 -Wl,--defsym,IRQ_STACK_SIZE=1024 -Wl,--defsym,SYS_STACK_SIZE=0 -L WICED/platform/MCU/BCM4390x/BCM43907 -L WICED/platform/MCU/BCM4390x -Wl,-T ././WICED/platform/MCU/BCM4390x/GCC/dct.ld -Wl,-Map,build/tgt_wifi-XYZ_LV_MCU-debug/APPS.map -o build/tgt_wifi-XYZ_LV_MCU-debug/APPS.elf build/tgt_wifi-XYZ_LV_MCU-debug/apps_header.o
SEGGER J-Link Commander V6.34a (Compiled Aug 8 2018 16:37:19)
DLL version V6.34a, compiled Aug 8 2018 16:36:42
J-Link Command File read successfully.
Processing script file...
J-Link connection not established yet but required for command.
Connecting to J-Link via USB...O.K.
Firmware: J-Link V10 compiled Jul 23 2018 09:53:14
Hardware version: V10.10
S/N: 12345678
License(s): GDB
VTref=3.303V
Target connection not established yet but required for command.
Device "CYW43907" selected.
Connecting to target via JTAG
TotalIRLen = 4, IRPrint = 0x01
JTAG chain detection found 1 devices:
#0 Id: 0x5BA00477, IRLen: 04, CoreSight JTAG-DP
Scanning AP map to find all available APs
AP[2]: Stopped AP scan as end of AP map has been reached
AP[0]: APB-AP (IDR: 0x44770002)
AP[1]: JTAG-AP (IDR: 0x24760010)
Iterating through AP map to find AHB-AP to use
AP[0]: APB-AP found
ROMTbl[0][0]: CompAddr: 80001000 CID: B105900D, PID:04-008BBC14 Cortex-R4
Found Cortex-R4 r1p4
4 code breakpoints, 4 data breakpoints
Debug architecture ARMv7.0
Data endian: little
Main ID register: 0x411FC144
I-Cache L1: 32 KB, 256 Sets, 32 Bytes/Line, 4-Way
D-Cache L1: 32 KB, 256 Sets, 32 Bytes/Line, 4-Way
TCM Type register: 0x00010001
MPU Type register: 0x00000800
System control register:
Instruction endian: little
Level-1 instruction cache enabled
Level-1 data cache enabled
MPU enabled
Branch prediction enabled
Memory zones:
[0]: Default (Default access mode)
[1]: APB-AP (AP0) (DMA like acc. in AP0 addr. space)
Cortex-R4 identified.
Reset delay: 0 ms
Reset type NORMAL: Toggle reset pin and halt CPU core.
J-Link script: Reset
J-Link script: Done
Writing 00000000 -> 18020634
Downloading file [build/tgt_wifi-XYZ_LV_MCU-debug/DCT.bin]...
Unspecified error -1
Script processing completed.
echo Downloading Bootloader ...
Downloading Bootloader ...
C:\Tool\SEGGER\JLink_V634a\JLink.exe -device CYW43907 -if JTAG -speed auto -jtagconf -1,-1 -autoconnect 1 -CommanderScript jlink_commander_script.txt
SEGGER J-Link Commander V6.34a (Compiled Aug 8 2018 16:37:19)
DLL version V6.34a, compiled Aug 8 2018 16:36:42
J-Link Command File read successfully.
Processing script file...
J-Link connection not established yet but required for command.
Connecting to J-Link via USB...O.K.
Firmware: J-Link V10 compiled Jul 23 2018 09:53:14
Hardware version: V10.10
S/N: 12345678
License(s): GDB
VTref=3.303V
Target connection not established yet but required for command.
Device "CYW43907" selected.
Connecting to target via JTAG
TotalIRLen = 4, IRPrint = 0x01
JTAG chain detection found 1 devices:
#0 Id: 0x5BA00477, IRLen: 04, CoreSight JTAG-DP
Scanning AP map to find all available APs
AP[2]: Stopped AP scan as end of AP map has been reached
AP[0]: APB-AP (IDR: 0x44770002)
AP[1]: JTAG-AP (IDR: 0x24760010)
Iterating through AP map to find AHB-AP to use
AP[0]: APB-AP found
ROMTbl[0][0]: CompAddr: 80001000 CID: B105900D, PID:04-008BBC14 Cortex-R4
Found Cortex-R4 r1p4
4 code breakpoints, 4 data breakpoints
Debug architecture ARMv7.0
Data endian: little
Main ID register: 0x411FC144
I-Cache L1: 32 KB, 256 Sets, 32 Bytes/Line, 4-Way
D-Cache L1: 32 KB, 256 Sets, 32 Bytes/Line, 4-Way
TCM Type register: 0x00010001
MPU Type register: 0x00000800
System control register:
Instruction endian: little
Level-1 instruction cache enabled
Level-1 data cache enabled
MPU enabled
Branch prediction enabled
Memory zones:
[0]: Default (Default access mode)
[1]: APB-AP (AP0) (DMA like acc. in AP0 addr. space)
Cortex-R4 identified.
Reset delay: 0 ms
Reset type NORMAL: Toggle reset pin and halt CPU core.
J-Link script: Reset
J-Link script: Done
Writing 00000000 -> 18020634
Downloading file [build/waf.bootloader-NoOS-NoNS-XYZ_LV_MCU-REV_B-SoC.43909/binary/waf.bootloader-NoOS-NoNS-XYZ_LV_MCU-REV_B-SoC.43909.trx.bin]...
Unspecified error -1
Script processing completed.
****** Error: Could not start CPU core. (ErrorCode: -1)
echo Finished Downloading Bootloader
Finished Downloading Bootloader
"./tools/ARM_GNU/Win32/bin/arm-none-eabi-strip.exe" -o build/tgt_wifi-XYZ_LV_MCU-debug/APPS.stripped.elf build/tgt_wifi-XYZ_LV_MCU-debug/APPS.elf
echo Downloading resources filesystem ... build/tgt_wifi-XYZ_LV_MCU-debug/filesystem.bin at sector 17
size 125...
Downloading resources filesystem ... build/tgt_wifi-XYZ_LV_MCU-debug/filesystem.bin at sector 17 size 125...
C:\Tool\SEGGER\JLink_V634a\JLink.exe -device CYW43907 -if JTAG -speed auto -jtagconf -1,-1 -autoconnect 1 -CommanderScript jlink_commander_script.txt
SEGGER J-Link Commander V6.34a (Compiled Aug 8 2018 16:37:19)
DLL version V6.34a, compiled Aug 8 2018 16:36:42
J-Link Command File read successfully.
Processing script file...
J-Link connection not established yet but required for command.
Connecting to J-Link via USB...O.K.
Firmware: J-Link V10 compiled Jul 23 2018 09:53:14
Hardware version: V10.10
S/N: 12345678
License(s): GDB
VTref=3.322V
Target connection not established yet but required for command.
Device "CYW43907" selected.
Connecting to target via JTAG
TotalIRLen = 4, IRPrint = 0x01
JTAG chain detection found 1 devices:
#0 Id: 0x5BA00477, IRLen: 04, CoreSight JTAG-DP
Scanning AP map to find all available APs
AP[2]: Stopped AP scan as end of AP map has been reached
AP[0]: APB-AP (IDR: 0x44770002)
AP[1]: JTAG-AP (IDR: 0x24760010)
Iterating through AP map to find AHB-AP to use
AP[0]: APB-AP found
ROMTbl[0][0]: CompAddr: 80001000 CID: B105900D, PID:04-008BBC14 Cortex-R4
Found Cortex-R4 r1p4
4 code breakpoints, 4 data breakpoints
Debug architecture ARMv7.0
Data endian: little
Main ID register: 0x33040014
Unified-Cache L1: 0 KB, 32768 Sets, 2048 Bytes/Line, 1024-Way
D-Cache L2: 0 KB, 32768 Sets, 2048 Bytes/Line, 1024-Way
TCM Type register: 0x00CC1000
MPU Type register: 0x00CC1000
System control register:
Instruction endian: little
Level-1 instruction cache enabled
Level-1 data cache disabled
MPU disabled
Branch prediction disabled
****** Error: Could not read CP15 register.
Cannot connect to target.
Target connection not established yet but required for command.
Device "CYW43907" selected.
Connecting to target via JTAG
Cannot connect to target.
Script processing completed.
"./tools/ARM_GNU/Win32/bin/arm-none-eabi-objcopy.exe" -O binary -R .eh_frame -R .init -R .fini -R .comment -R .ARM.attributes build/tgt_wifi-XYZ_LV_MCU-debug/APPS.stripped.elf build/tgt_wifi-XYZ_LV_MCU-debug/APPS.bin
echo Downloading APP0 build/tgt_wifi-XYZ_LV_MCU-debug/binary/tgt_wifi-XYZ_LV_MCU-debug.stripped.elf @ sector 142 address 581632 size 66...
Downloading APP0 build/tgt_wifi-XYZ_LV_MCU-debug/binary/tgt_wifi-XYZ_LV_MCU-debug.stripped.elf @ sector 142 address 581632 size 66...
C:\Tool\SEGGER\JLink_V634a\JLink.exe -device CYW43907 -if JTAG -speed auto -jtagconf -1,-1 -autoconnect 1 -CommanderScript jlink_commander_script.txt
SEGGER J-Link Commander V6.34a (Compiled Aug 8 2018 16:37:19)
DLL version V6.34a, compiled Aug 8 2018 16:36:42
J-Link Command File read successfully.
Processing script file...
J-Link connection not established yet but required for command.
Connecting to J-Link via USB...O.K.
Firmware: J-Link V10 compiled Jul 23 2018 09:53:14
Hardware version: V10.10
S/N: 12345678
License(s): GDB
VTref=3.322V
Target connection not established yet but required for command.
Device "CYW43907" selected.
Connecting to target via JTAG
TotalIRLen = 4, IRPrint = 0x01
JTAG chain detection found 1 devices:
#0 Id: 0x5BA00477, IRLen: 04, CoreSight JTAG-DP
Scanning AP map to find all available APs
AP[2]: Stopped AP scan as end of AP map has been reached
AP[0]: APB-AP (IDR: 0x44770002)
AP[1]: JTAG-AP (IDR: 0x24760010)
Iterating through AP map to find AHB-AP to use
AP[0]: APB-AP found
ROMTbl[0][0]: CompAddr: 80001000 CID: B105900D, PID:04-008BBC14 Cortex-R4
Found Cortex-R4 r1p4
4 code breakpoints, 4 data breakpoints
Debug architecture ARMv7.0
Data endian: little
Main ID register: 0x33040014
Unified-Cache L1: 0 KB, 32768 Sets, 2048 Bytes/Line, 1024-Way
D-Cache L2: 0 KB, 32768 Sets, 2048 Bytes/Line, 1024-Way
TCM Type register: 0x00CC1000
MPU Type register: 0x00CC1000
System control register:
Instruction endian: little
Level-1 instruction cache enabled
Level-1 data cache disabled
MPU disabled
Branch prediction disabled
****** Error: Could not read CP15 register.
Cannot connect to target.
Target connection not established yet but required for command.
Device "CYW43907" selected.
Connecting to target via JTAG
Cannot connect to target.
Script processing completed.
echo Downloading apps lookup table in wiced_apps.mk ... build/tgt_wifi-XYZ_LV_MCU-debug/APPS.bin @ 0x00010000 size
Downloading apps lookup table in wiced_apps.mk ... build/tgt_wifi-XYZ_LV_MCU-debug/APPS.bin @ 0x00010000 size
C:\Tool\SEGGER\JLink_V634a\JLink.exe -device CYW43907 -if JTAG -speed auto -jtagconf -1,-1 -autoconnect 1 -CommanderScript jlink_commander_script.txt
SEGGER J-Link Commander V6.34a (Compiled Aug 8 2018 16:37:19)
DLL version V6.34a, compiled Aug 8 2018 16:36:42
J-Link Command File read successfully.
Processing script file...
J-Link connection not established yet but required for command.
Connecting to J-Link via USB...O.K.
Firmware: J-Link V10 compiled Jul 23 2018 09:53:14
Hardware version: V10.10
S/N: 12345678
License(s): GDB
VTref=3.322V
Target connection not established yet but required for command.
Device "CYW43907" selected.
Connecting to target via JTAG
TotalIRLen = 4, IRPrint = 0x01
JTAG chain detection found 1 devices:
#0 Id: 0x5BA00477, IRLen: 04, CoreSight JTAG-DP
Scanning AP map to find all available APs
AP[2]: Stopped AP scan as end of AP map has been reached
AP[0]: APB-AP (IDR: 0x44770002)
AP[1]: JTAG-AP (IDR: 0x24760010)
Iterating through AP map to find AHB-AP to use
AP[0]: APB-AP found
ROMTbl[0][0]: CompAddr: 80001000 CID: B105900D, PID:04-008BBC14 Cortex-R4
Found Cortex-R4 r1p4
4 code breakpoints, 4 data breakpoints
Debug architecture ARMv7.0
Data endian: little
Main ID register: 0x33040014
Unified-Cache L1: 0 KB, 32768 Sets, 2048 Bytes/Line, 1024-Way
D-Cache L2: 0 KB, 32768 Sets, 2048 Bytes/Line, 1024-Way
TCM Type register: 0x00CC1000
MPU Type register: 0x00CC1000
System control register:
Instruction endian: little
Level-1 instruction cache enabled
Level-1 data cache disabled
MPU disabled
Branch prediction disabled
****** Error: Could not read CP15 register.
Cannot connect to target.
Target connection not established yet but required for command.
Device "CYW43907" selected.
Connecting to target via JTAG
Cannot connect to target.
Script processing completed.
echo Resetting target
Resetting target
C:\Tool\SEGGER\JLink_V634a\JLink.exe -device CYW43907 -if JTAG -speed auto -jtagconf -1,-1 -autoconnect 1 -CommanderScript jlink_commander_script.txt
SEGGER J-Link Commander V6.34a (Compiled Aug 8 2018 16:37:19)
DLL version V6.34a, compiled Aug 8 2018 16:36:42
J-Link Command File read successfully.
Processing script file...
J-Link connection not established yet but required for command.
Connecting to J-Link via USB...O.K.
Firmware: J-Link V10 compiled Jul 23 2018 09:53:14
Hardware version: V10.10
S/N: 12345678
License(s): GDB
VTref=3.322V
Target connection not established yet but required for command.
Device "CYW43907" selected.
Connecting to target via JTAG
TotalIRLen = 4, IRPrint = 0x01
JTAG chain detection found 1 devices:
#0 Id: 0x5BA00477, IRLen: 04, CoreSight JTAG-DP
Scanning AP map to find all available APs
AP[2]: Stopped AP scan as end of AP map has been reached
AP[0]: APB-AP (IDR: 0x44770002)
AP[1]: JTAG-AP (IDR: 0x24760010)
Iterating through AP map to find AHB-AP to use
AP[0]: APB-AP found
ROMTbl[0][0]: CompAddr: 80001000 CID: B105900D, PID:04-008BBC14 Cortex-R4
Found Cortex-R4 r1p4
4 code breakpoints, 4 data breakpoints
Debug architecture ARMv7.0
Data endian: little
Main ID register: 0x33040014
Unified-Cache L1: 0 KB, 32768 Sets, 2048 Bytes/Line, 1024-Way
D-Cache L2: 0 KB, 32768 Sets, 2048 Bytes/Line, 1024-Way
TCM Type register: 0x00CC1000
MPU Type register: 0x00CC1000
System control register:
Instruction endian: little
Level-1 instruction cache enabled
Level-1 data cache disabled
MPU disabled
Branch prediction disabled
****** Error: Could not read CP15 register.
Cannot connect to target.
Target connection not established yet but required for command.
Device "CYW43907" selected.
Connecting to target via JTAG
Cannot connect to target.
Target connection not established yet but required for command.
Device "CYW43907" selected.
Connecting to target via JTAG
Cannot connect to target.
Script processing completed.
make.exe[1]: Leaving directory 'C:/Projekte/XYZ/xyz_tgt_wifi/43xxx_Wi-Fi'
echo Build complete
Build complete
echo Making .gdbinit
Making .gdbinit
echo set remotetimeout 20 > .gdbinit
echo shell start /B ./tools/OpenOCD/Win32/openocd-all-brcm-libftdi.exe -s ./tools/OpenOCD/scripts -f ./tools/OpenOCD/jlink-native.cfg -f ./tools/OpenOCD/BCM4390x.cfg -f ./tools/OpenOCD/BCM4390x_gdb_jtag.cfg -l build/openocd_log.txt >> .gdbinit
echo shell ping 127.0.0.1 -n 5 >> .gdbinit
make: Leaving directory 'C:/Projekte/XYZ/xyz_tgt_wifi/43xxx_Wi-Fi'
Hi, can this be extended to CY4343x STM32 based devices?
rroy
J-Link native support is really nice!! Looks this is only for 43907 at this moment. Any plan to support other MCUs? If you can support STM32 as well, it would be great.