Announcements
IMPORTANT: Cypress Developer Community currently doesn’t allow sign-in to prepare for the upcoming transition. To learn more, check out our announcement.
cancel
Showing results for 
Search instead for 
Did you mean: 

Wi-Fi Combo

Anonymous
Not applicable

Hello,

My application requires fairly high speed data acquisition (4Gb/s).  To do this in absence of some integrated solution, we use FPGAs.  This gives us basically Cortex A9, Xilinx Microblaze, or Altera NIOS as possible processors.  The market is not huge.  Perhaps a few 10Ks/year.  However, if I don't ask, I can assure not possible support.

Regards,

davidhil

0 Likes
2 Replies
SeyhanA_31
Employee

Hi,

Are you looking for a support on WiFi interface for either Cortex A9, Xilinx Microblaze, or Altera NIOS on FPGA?

What OS are you planning to run on your selected processor?

Seyhan

0 Likes
Anonymous
Not applicable

Hello Seyhan,

Probably FreeRTOS works as well as anything.  Currently I've a Microblaze, and the current setup probably won't work, because it hasn't enough RAM to support any RTOS at all + app (128K total memory).  So, any of the three would ultimately be acceptable.  I've verified that (at least on Xilinx A9) I can port.  I haven't tried porting to Altera. Probably, your best solution would be the A9 since it is common to both the Altera and Xilinx community.

My problem is that we have data paths that are MUCH faster than can easily be supported by any processor system (sort of 4Gb/sec minimum per active channel; 4 channels max).  This means we always have an FPGA (or an ASIC). And, preference is always to have the data memory inside the address space of the processor to avoid weird data access problems.


On rethinking this slightly, it is likely that I can make a Microblaze work using Execute in Place out of programming flash.  Clearly, some form of cache would be useful for that.  I haven't data on Altera's XiP capabilities, but suspect this might be a solution there as well.  This also reduces the RAM overhead on the A9 solutions, probably meaning that the L2 cache can provide enough RAM for the true variables (and maybe for commonly used code as well).


IF this actually is feasible (I don't see this getting tested soon, so let's assume it works), than any of the solutions (A9, Microblaze or NIOS) is viable.

Regards,

Dave

0 Likes