cancel
Showing results for 
Search instead for 
Did you mean: 

Wi-Fi Combo

Anonymous
Not applicable

Hi,

We have a LED to indicate if data is transfering on the wifi link or not.

Does SDK support the API or callback to get the status?

0 Likes
1 Reply
Anonymous
Not applicable

There are no explicit APIs at this moment to indicate that data is being sent over the air. The closest approximation that you could leverage would be to hook into one of the bus functions like - wwd_bus_sdio_transfer - which will indicate valid packets being transferred to and from the WiFi MAC layer.

This is a hacky way to accomplish what you want however.

Recommend - that you instead hook into the wwd_thread_receive_one_packet and wwd_thread_send_one_packet to mimic the functionality

Keep in mind that all of these are low-level functions and may potentially change between SDK revisions