The datasheet for the 1MW has 7 programmable GPIO pins. Are any of them configurable to provide a WIFI HOST WAKE UP interrupt?
Solved! Go to Solution.
In case of WICED SDK, the datasheet from Cypress does not mention that pin, but on the Cypress platform, GPIO_0 is allocated for WL_HOST_WAKE, so I believe GPIO_0 can is the one. You need to engage with Cypress to have WL_HOST_WAKE on another pin.
You can see the schematics in this folder: 43xxx_Wi-Fi\platforms\CYW943455EVB_02\schematics.
In case of WICED SDK, the datasheet from Cypress does not mention that pin, but on the Cypress platform, GPIO_0 is allocated for WL_HOST_WAKE, so I believe GPIO_0 can is the one. You need to engage with Cypress to have WL_HOST_WAKE on another pin.
You can see the schematics in this folder: 43xxx_Wi-Fi\platforms\CYW943455EVB_02\schematics.
Thanks for the info. I am not sure what you are referencing with the folder. Is this part of the WICED SDK installation? I don't have it installed yet!
Yes, I am referencing WICED SDK. You can download it from here: WICED Studio Wi-Fi/Combo Docs & Downloads
Thanks for your help. My question has been answered!!