Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Hi,

I'm using SN8000x EVB from Murata + Wiced SDK 3.1.0, I want to use the SDIO on that board for sd card interfacing. From the SDK I can see a

wiced_result_t wiced_init( void )

{

    WPRINT_WICED_INFO( ("\nStarting WICED v" WICED_VERSION "\n") );

    CHECK_RETURN( wiced_core_init( ) );

    //CHECK_RETURN( wiced_wlan_connectivity_init( ) );

    return WWD_SUCCESS;

}

I commented out the  wiced_wlan_connectivity_init( ) function which initialize WLAN driver...


Is there anything else that I need to do so that I can isolate the SDIO port from WLAN using it and proceed using SDIO for my SD card interface....

0 Likes
1 Reply
VikramR_26
Employee
Employee
25 sign-ins 10 sign-ins 10 comments on KBA

Within wiced_core there is wiced_core_init() -->    wiced_platform_init( ); this initializes the platform related to hardware interfaces...

0 Likes