Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Hi,

This is going to sound like madness but I can't really find a straight answer: Can you actually develop directly for the 43362? There is certainly a strong emphasis on using it as an SPI peripheral, but can it be run standalone?

Thanks,

Dave

0 Likes
4 Replies
Anonymous
Not applicable

Sure, that's what the snapper board from ackme is for ACKme | AMW004-E01 (Snapper)

and if you look at the module itself you can see the block diagram ACKme | AMW004 (Wallaby)

hope that helps...

SeyhanA_31
Employee
Employee
250 replies posted 100 replies posted 50 replies posted

Hi David,

Is your question about BCM43362 chip (radio) or BCM943362 module (radio + host CPU)?

Thanks,

Seyhan

0 Likes
Anonymous
Not applicable

Seyhan,

The chip, I was proposing to use the Murata SN8000 module.

-Dave

0 Likes

Hi,

The BCM43362 communicates to host CPU via SDOI/SPI. Host CPU implements network and security stacks, protocols, etc. Murata SN8000 module supports host CPUs with WICED SDK, please check SN8000 2.4GHz Wi-Fi 802.11b/g/n. The BCM43362 with host CPU module could be run standalone. Please check Broadcom partners for such modules Partners.

-Seyhan

0 Likes