Dev under OS X

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Hello guys,

i've recently bought dev board from Stm Discowery Wifi which includes SN8200 module. Self St suggest to use it only with Discovery32F4 dev board and all their guides are only describing them in pair, but i want use only SN8200 as it all-in module.

I have installed WICED 2.4.1 on my mac, and  connect SN8200 with Usb to ttl converter connected to uart, but i can't find in Wiced IDE menu my board.  Maybe can someone help me?

Also in Starting Guide in description of board testing named snip_ping_.. file which also can't find in Wiced IDE.

Thank you in advance for your help.

0 Likes
3 Replies
SeyhanA_31
Employee
Employee
250 replies posted 100 replies posted 50 replies posted

Sergii,

Please take a look at this discussion: http://community.broadcom.com/message/1953#1953

"There is a patch file available on the Murata portal for the SN8200.  Please register with your EVK registration code at www.murata-ws.com."

-Seyhan

0 Likes
GregG_16
Employee
Employee
50 sign-ins 25 sign-ins 25 comments on KBA

Usually module suppliers provide "platform files" these will patch into our SDK.

0 Likes

Sergii,

Perhaps you could use the rar file to update your SDK and you may find here: http://www.murata-ws.com./software/SN820x-WICED-2.4.0-patch-02.rar

Even the patch file is for version 2.4.0 but it should work for 2.4.1 as well.

Hope it helps.

Seyhan