cancel
Showing results for 
Search instead for 
Did you mean: 

Wi-Fi Combo

ericboxer_
New Contributor II

I am trying to connect the CYW to an Enterprise network using peap after loading the test.console app on the device. Ive replaced the root cert in certificate.h and run the join_ent command:

joint_ent MYSSID peap MYUSER MYPASSWORD wpa2

Just returns an empty console input. Using the same SSID in the join command at least lets me know that it has failed to connect.

The credentials I'm using do work as I have used my a couple of computers both be able to join using them.

Not entering the correct number of arguments does at least return an "INSUFFICIENT ARGUMENTS" error.

Is there anything else I should try?

0 Likes
1 Solution
AxLi_1746341
Honored Contributor

ErBo_4350271 wrote:

I am trying to connect the CYW to an Enterprise network using peap after loading the test.console app on the device. Ive replaced the root cert in certificate.h and run the join_ent command:

  1. joint_ent MYSSID peap MYUSER MYPASSWORD wpa2 

There is a typo in your command. Use join_ent instead of joint_ent.

View solution in original post

1 Reply
AxLi_1746341
Honored Contributor

ErBo_4350271 wrote:

I am trying to connect the CYW to an Enterprise network using peap after loading the test.console app on the device. Ive replaced the root cert in certificate.h and run the join_ent command:

  1. joint_ent MYSSID peap MYUSER MYPASSWORD wpa2 

There is a typo in your command. Use join_ent instead of joint_ent.

View solution in original post