cancel
Showing results for 
Search instead for 
Did you mean: 

Wi-Fi Combo

NiMc_1688136
Contributor II

When running FreeRTOS with powersave disabled, what clock source provides the tick through platform_tick_isr? Is it the external 32.768 KHz crystal, LPO, or is it derived from the oscillator that is internal to the 1GC module?

Out of thousands of devices shipped we are seeing one that has about 17% error and another that has about 10% error in a periodic scheduled event triggered through a FreeRTOS timer.

0 Likes
1 Solution
AditiB_81
Moderator
Moderator

Hi,

The clock source that provides the tick through platform_tick_isr is internal to the 1GC module with powersave disabled. The oscillator is internal to the 1GC module with the default frequency of 37.4 MHz.

Thanks

View solution in original post

1 Reply
AditiB_81
Moderator
Moderator

Hi,

The clock source that provides the tick through platform_tick_isr is internal to the 1GC module with powersave disabled. The oscillator is internal to the 1GC module with the default frequency of 37.4 MHz.

Thanks

View solution in original post