- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi
I use cyw43364 with wiced.
I want to use coex with third-party ble.
I want to disable SECI Coex and to enable 3 wire Coex.
below is array in wifi_nvram_image.h.
Q1. I can't find nvram.txt. So I will change below parameter. Is this right?
Q2. How should I change?
Q3. What GPIO is coex pin?
static const char wifi_nvram_image[] =
// # The following parameter values are just placeholders, need to be updated.
"manfid=0x2d0" "\x00"
"prodid=0x0726" "\x00"
"vendid=0x14e4" "\x00"
"devid=0x43e2" "\x00"
"boardtype=0x0726" "\x00"
"boardrev=0x1101" "\x00"
"boardnum=22" "\x00"
"xtalfreq=26000" "\x00"
"sromrev=11" "\x00"
"boardflags=0x00404000" "\x00"
"boardflags3=0x08000000" "\x00"
NVRAM_GENERATED_MAC_ADDRESS "\x00"
"nocrc=1" "\x00"
"ag0=255" "\x00"
"aa2g=1" "\x00"
"ccode=ALL"
"\x00"
//#Antenna diversity
"swdiv_en=1" "\x00"
"swdiv_gpio=2" "\x00"
"pa0itssit=0x20" "\x00"
"extpagain2g=0" "\x00"
//#PA parameters for 2.4GHz, measured at CHIP OUTPUT
"pa2ga0=-140,6566,-728" "\x00"
"AvVmid_c0=0x0,0xc8" "\x00"
"cckpwroffset0=5" "\x00"
//# PPR params
"maxp2ga0=84" "\x00"
"txpwrbckof=6" "\x00"
"cckbw202gpo=0" "\x00"
"legofdmbw202gpo=0x66111111" "\x00"
"mcsbw202gpo=0x77711111" "\x00"
"propbw202gpo=0xdd" "\x00"
//# OFDM IIR :
"ofdmdigfilttype=18" "\x00"
"ofdmdigfilttypebe=18" "\x00"
//# PAPD mode:
"papdmode=1" "\x00"
"papdvalidtest=1" "\x00"
"pacalidx2g=32" "\x00"
"papdepsoffset=-36" "\x00"
"papdendidx=61" "\x00"
//# LTECX flags
// "ltecxmux=1" "\x00"
//"ltecxpadnum=0x02030401" "\x00"
// "ltecxfnsel=0x3003" "\x00"
// "ltecxgcigpio=0x3012" "\x00"
//#il0macaddr=00:90:4c:c5:12:38
"wl0id=0x431b" "\x00"
"btcxwarflags=0x3" "\x00"
"deadman_to=0xffffffff" "\x00"
//# muxenab: 0x1 for UART enable, 0x2 for GPIOs, 0x8 for JTAG, 0x10 for HW OOB
"muxenab=0x11" "\x00"
//# CLDO PWM voltage settings - 0x4 - 1.1 volt
//#cldo_pwm=0x4 "\x00"
//#VCO freq 326.4MHz
"spurconfig=0x3" "\x00"
"\x00\x00";
Solved! Go to Solution.
- Labels:
-
WICED Studio
-
Wifi+Bluetooth
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Dear Customer,
Kindly get in touch with your module vendor to get the necessary support. Customers are not recommended to modify nvram parameters at all. Here are some relevant documentation:
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Dear Customer,
Kindly get in touch with your module vendor to get the necessary support. Customers are not recommended to modify nvram parameters at all. Here are some relevant documentation: