Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
alorc_4110946
Level 1
Level 1
First like received

make.exe[1]: *** No rule to make target 'apps/ww101/02/02_blinkled/../../ARM_CM4/crt0_GCC.c', needed by 'build/ww101.02.02_blinkled-CYW94343WWCD1_EVB/Modules/apps/ww101/02/02_blinkled/../../ARM_CM4/crt0_GCC.o'.  Stop.

make.exe[1]: *** Waiting for unfinished jobs....

Building Bootloader

Finished Building Bootloader

Makefile:351: recipe for target 'main_app' failed

make: *** [main_app] Error 2

MK file:

Name := apps_ww101_02_04_button

$(NAME)_SOURCES := 04_button.c

c file

#include "wiced.h"

void application_start()

{

    wiced_init();

        while(1)

        {

            button1_pressed = wiced_gpio_input_get(WICED_BUTTON1) ? WICED_FALSE : WICED_TRUE;

            if(button1_pressed == WICED_TRUE)

            {

                wiced_gpio_output_high (WICED_LED1);

            }

            else

            {

                wiced_gpio_output_low (WICED_LED1);

            }

        }

}

File structure:

0 Likes
1 Solution

Was able to work through. Thank you for help. Can close "Case"

View solution in original post

5 Replies
RaktimR_11
Moderator
Moderator
Moderator
500 replies posted 250 replies posted 100 replies posted

Which WICED Studio version are you using? Can you check in your system whether the ARM_CM4 directory exists in the following location 43xxx_Wi-Fi/WICED/platform/ARM_CM4?

I ran the example from CypressAcademy_WW101_Files/04_button.mk at master · cypresssemiconductorco/CypressAcademy_WW101_File... and was able to compile successfully.

Hello RaktimR-

Thank you for the response.

The following is answers

Downloaded

WICED Studio Wi-Fi/Combo v6.x SDKs

* WICED Studio 6.2.1

WICED-Studio 6.2.1 Installer (Windows)

ARM_CM4 in this directory

C:\Users\Al\Documents\WICED-

Studio-6.2\temp\43xxx_Wi-Fi\WICED\platform\ARM_CM4
CMSIS

                 3/21/2019       10:49:42 PM
  crt0_GCC.c

         8 KB    3/21/2019       10:49:42 PM
  crt0_IAR.c

         4 KB    3/21/2019       10:49:42 PM
  hardfault_handler.c

         16 KB   3/21/2019       10:49:42 PM
  host_cm7.c

         3 KB    3/21/2019       10:49:42 PM
  platform_assert.h

         5 KB    3/21/2019       10:49:42 PM
  platform_checkpoint.h

         5 KB    3/21/2019       10:49:42 PM
  platform_isr.h

         7 KB    3/21/2019       10:49:42 PM

--AAO

0 Likes

Are you still seeing the error?

0 Likes

Still see errors

If I copy a snip file from the make Target as follows using the platform CYW94343WWCD1

     snip.scan-CYW94343WWCD1_EVB download all builds OK. blinkled worked. Button has issues as below.

Complete files and output is as follows for button exercise in the tutorial. Same happens with blinkled exerise:

ww101.02.04_button-CYW94343WWCD1_EVB download

04_button.mk

NAME := apps_ww101_02_04_button

$(NAME)_SOURCES := 04_button.c

04_button.c  -

#include "wiced.h"

void application_start( )

{

wiced_init( );

while(1)

{

            button1_pressed = wiced_gpio_input_get(WICED_BUTTON1) ? WICED_FALSE : WICED_TRUE;

            if(button1_pressed == WICED_TRUE)

            {

                wiced_gpio_output_high (WICED_LED1);

            }

            else

            {

                wiced_gpio_output_low (WICED_LED1);

            }

}

}

ERROR

20:35:09 **** Build of configuration Default for project 43xxx_Wi-Fi ****

"C:\\Users\\Al\\Documents\\WICED-Studio-6.2\\43xxx_Wi-Fi\\make.exe" ww101.02.04_button-CYW94343WWCD1_EVB download

MAKEFILE MAKECMDGOALS=ww101.02.04_button-CYW94343WWCD1_EVB download OTA2_SUPPORT is disabled

Building Bootloader

Building Serial Flash Loader App

MAKEFILE MAKECMDGOALS=waf.sflash_write-NoOS-CYW94343WWCD1_EVB-SDIO OTA2_SUPPORT is disabled

  1. waf.sflash_write-NoOS-CYW94343WWCD1_EVB-SDIO

----------------------------------|---------|

                                  |  Static |

              Module              |   RAM |

----------------------------------+---------|

App                               |   21130 |

Host MCU-family library           | 11604 |

Interrupt Vectors                 |     388 |

libc                              |     556 |

platform                          |    1104 |

Ring_Buffer                       |      40 |

SPI_Flash_Library_CYW94343WWCD1_EV|     936 |

Startup Stack & Link Script fill  |     486 |

WWD                               |     188 |

----------------------------------+---------|

TOTAL (bytes)                     |   36432 |

----------------------------------|---------|

Build complete

Finished Building Bootloader

Finished Building Serial Flash Loader App

Compiling apps_ww101_02_04_button

apps/ww101/02/04_button/04_button.c: In function 'application_start':

apps/ww101/02/04_button/04_button.c:9:13: error: 'button1_pressed' undeclared (first use in this function)

             button1_pressed = wiced_gpio_input_get(WICED_BUTTON1) ? WICED_FALSE : WICED_TRUE;

             ^~~~~~~~~~~~~~~

apps/ww101/02/04_button/04_button.c:9:13: note: each undeclared identifier is reported only once for each function it appears in

tools/makefiles/wiced_elf.mk:232: recipe for target 'build/ww101.02.04_button-CYW94343WWCD1_EVB/Modules/apps/ww101/02/04_button/04_button.o' failed

  1. make.exe[1]: *** [build/ww101.02.04_button-CYW94343WWCD1_EVB/Modules/apps/ww101/02/04_button/04_button.o] Error 1
  2. make.exe[1]: *** Waiting for unfinished jobs....

make: *** [main_app] Error 2

Makefile:351: recipe for target 'main_app' failed

20:35:50 Build Finished (took 41s.215ms)

Was able to work through. Thank you for help. Can close "Case"