cancel
Showing results for 
Search instead for 
Did you mean: 

Wi-Fi Combo

Anonymous
Not applicable
I noticed that, in linux brcm wifi driver, structure bdc_header defined as below:

struct bdc_header {

uint8 flags;   /* Flags */

uint8 priority; /* 802.1d Priority 0:2 bits, 4:7 flow control info for usb */

uint8 flags2;

uint8 rssi;

};

but in wiced implementation,bdc_header defined as :

typedef struct

{

    uint8_t flags;      /* Flags */

    uint8_t priority;   /* 802.1d Priority (low 3 bits) */

    uint8_t flags2;

    uint8_t data_offset; /* Offset from end of BDC header to packet data, in 4-uint8_t words.  Leaves room for optional headers.*/

} sdpcm_bdc_header_t;

The last member is changed to data_offset, it is bad .

RSSI is very important information, where can I find this info instead?
0 Likes
1 Solution
Anonymous
Not applicable
Whats wrong with using the wiced_wifi_get_rssi() API call?

View solution in original post

0 Likes
3 Replies
Anonymous
Not applicable
Whats wrong with using the wiced_wifi_get_rssi() API call?

View solution in original post

0 Likes
GregG_16
Employee

Is this still an issue?

0 Likes
Anonymous
Not applicable

Discussion is being locked. If you have any follow-up, please start a new discussion.

0 Likes