- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
The snip.uart in the WICED SDK 3.3.1 uses STDIO_UART to echo bytes sent over the terminal connected to that COM port.
I want to repurpose that application to use pins 9 and 10 on the breakout header. These stand for UART2 RX and TX respectively.
I want to know how can I pass the UART2 number in the wicked_uart_init()? As of now, the SDK has platform.h for BCM943341WCD1 has the following definition for UART
typedef enum
{
WICED_UART_1,
WICED_UART_MAX, /* Denotes the total number of UART port aliases. Not a valid UART alias */
WICED_UART_32BIT = 0x7FFFFFFF,
} wiced_uart_t;
/* UART port used for standard I/O */
#define STDIO_UART ( WICED_UART_1 )
Can I use WICED_UART_2 and hope that this will result in TX/RX on the respective pins 9 and 10. Is there anything else I need to configure besides adding WICED_UART2=2 in the wiced_uart_t structure and passing it to the init function below?
/* Initialise UART. A ring buffer is used to hold received characters */
wiced_uart_init( STDIO_UART, &uart_config, &rx_buffer );
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Arsh,
Hi.
Thanks. I was able to repurpose WICED_UART4 using the example posted here ...
Enable UART4 on BCM943362WCD4 and BCM943341WCD1 as Terminal Output
Regards,
Manish
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Your could check platform files of BCM943362WCD4 and/or BCM9WCDPLUS114 as reference!
Both already configure two UART port!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
WICED_UART_2 has not been connected to the FTDI chip. As a result, you will have to modify the hardware as well as the platform files.
Thanks,
Arsh Buch
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Arsh,
Hi.
Thanks. I was able to repurpose WICED_UART4 using the example posted here ...
Enable UART4 on BCM943362WCD4 and BCM943341WCD1 as Terminal Output
Regards,
Manish
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
BTW, we just want a regular UART ... not a terminal one with serial to USB or vice-versa conversion.