cancel
Showing results for 
Search instead for 
Did you mean: 

Wi-Fi Combo

Anonymous
Not applicable

Hi,

I recently got BCM43909KRFBG based development and 3.3.1 SDK , When I received I just tested the board everything was working  .. I tested few things of console app , like scan , join etc .. I tried the same app from the 3.3.1 SDK buy going through the README guide .

I jut tried the below command

$make test.console-BCM943909WCD1 download run

Everything went fine and the app got downloaded to the board ..

But when I run >scan , it was not able to scan any APs .. none of the wifi related commands are working ..

>status command showing that

WICED Version  : 3.3.1
Platform       : BCM943909WCD1
MAC Address    : EF:EF:EF:EF:EF:EF

STA Interface  : Down
AP Interface   : Down
P2P Interface  : Down
Ethernet Interface  : Down

Am  I need to enable anything to make wifi working ? is there any setting am missing ?

0 Likes
1 Reply
Anonymous
Not applicable

Hey,

Can you try with other demo applications that are provided with the SDK.

For instance,

demo.temp_control-BCM943909WCD1 download run

You may want to check out other demo applications.

Let us know if it works.


Best Regards,

AB

0 Likes