[43907]开启快速漫游

公告

大中华汽车电子生态圈社区并入开发者社区- 更多资讯点击此

Tip / 登入 to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
qiji_3572186
Level 1
Level 1
First question asked

我们现在使用的是43907模块,wiced 6.4

对漫游有比较高的要求,所以在漫游做scan的时候,只需要scan某几个指定的信道,比如说1,6,11。

我在论坛上有看到帖子说(Does someone know the details of roam scan?

   In addition if all the access points are set to channel 1, 6, 11,  we can preset the scan channels into 1, 6, 11 instead of all the 2.4G channels or 5G channels.  It will give a much quicker scan speed and improve the ratio of the roam.
   BG Channel Set:
  
Optional value: Full (all channels); 1,6,11 ; 1,7,13; or Custom

我在sdk中没有找到BG clannel set的设置的地方。

我看到在sdk中wiced_wifi_scan_networks_ex可以设置san的信道,wifi在漫游的时候是否是默认也扫描这些指定的信道,还是扫描全部信道。

如果扫描全部信道,需要怎样才能设置这个BG channel set。

   

0 点赞
1 回复
Zhengbao_Zhang
Moderator
Moderator
Moderator
250 sign-ins First comment on KBA 10 questions asked

Hello:

   I think we can support the feature  , but it is better to contact with local FAE to raise the request to maintain the firmware version , otherwise it will bring  more delay when supporting. 

0 点赞